• HMC874 clock input

    Hello,

           What kind of clock sources be used for the clock input of the device? Can a synthesizer like ADF4371 be used to drive it? If yes, please advise on the circuit else please suggest the appropriate approach. 

    Thank you for your help in advance,

  • There is no high-speed comparator HMC874 simulation model in LTSPICE. How can we simulate this product?

    I want to simulate this comparator, but I can't find its model in LTSIPCIE. Is there any way to simulate it?

  • 怎么仿真高速比较器HMC874?Ltspice中没有仿真模型

    找不到它的仿真模型

  • ADCMP572/ADCMP573 floating EPAD

    To Analog Devices Team:
    Guys, I beg you to change EPAD description in the datasheet. I lost almost a week to find the problem with grounded EPAD in ADCMP572. My rise/fall times were between 300ps to 400ps and after cutting ground I have achieved ~80ps…

  • We are looking for a high speed compactor which has the input equivalent BW up to 20GHz

    Hi EZ experts,

    We are looking for a high speed Compactor which has the equivalent BW up to 20GHz

    As we know, the highest  input equivalent BW is about 10GHz like HMC674 or HMC874.

    But our new application need a 20GHz input equivalent BW compactor, do you…

  • RE: HMC874LC3C

    HMC874 latches the INP-INN signal when it sees a rising edge. If you input a sine BPSK, it will latch at that signal's rising edge

  • RE: HMC874LC3C

    HMC874 latches the INP-INN signal when it sees a rising edge. If you input a sine BPSK, it will latch at that signal's rising edge

  • HMC874LC3C 输入带宽

    您好,我在阅读该芯片Datasheet后发现针对输入带宽范围没有明确说明,仅有一个等效输入带宽的范围,请问等效输入带宽的范围就是这个芯片的输入信号带宽范围(8.6~12GHz)嘛?

    期待您的解答~

  • RE: LMH7322 pulse stretch

    Hi drachir_1900,

    The sub nanosecond prop delay comparators are mostly characterized with IBIS models. Here is a list of devices from ADI for your reference:

     XLSX

    Regards,

    Hooman