• RE: HMC8410 Vdd range

    Hi mbarcak,

    I see that I answered this question for you via a 12/15/2016 email to Brian K (FAE, ADI), though I neglected to close out this EZ thread by also replying here in EZ. Perhaps the answer was not forwarded to you? Please see below and let me know…

  • 2HD, 3HD data of HMC441-Die and HMC462-Die

    Hi, 

    Could you share the 2nd and the 3rd harmonic distortion data?

    If there is no data of these products, something of the same product series is also fine.

    Regards,

    HM

  • HMC8410 sequencing options

    Hi,

    We are using HMC8410 Amplifier in our one of amplifier boards,

    In one of the post I did see that there was a recommendation of HMC981 or HMC920.

    Out of these two which would be best suitable for the HMC8410?

    If HMC981 to be used, the VG2 can be left…

  • HMC8410 biasing options

    Dear Sir/Madam:

    We are evaluating HMC8410 LNA chip.  It requires external active bias controller.

    Based on AN-1363, it suggest using HMC980, HMC981 and HMC920.

    Can you recommend which active bias controller should we use for HMC8410?  We would like to…

  • HMC8410 OIP2

    Hi, 

    From the datasheet, it seems like the OIP2 improves when the supply current increases. Is there any concerns if I increases the supply current from the recommended typical 65mA to about 100mA?

    Would also like to check for Figure 15 in the datasheet…

  • RE: HMC8410 supply

    Hi,

    Which is better HMC981LP3E or HMC920LP5E for the amplifier HMC8410?

    Kindly suggest, as there are 2 VG's are present in HMC981LP3E, what should be done with the VG2 (of HMC981LP3E) for the HMC8410?

    Thanks & Regards,

    Nanjunda M

  • HMC8410 Amplifier


    I am looking at this amplifier and would like to run some simulations on it if at all possible. However, I need the corresponding '.lib' and '.olb' files for PSPICE to recognize the amplifier. The corresponding S-parameter data sheet doesn't work for…

  • Question about HMC8410

    Hi,

    Is pin# 4 of HMC8410 NIC or Vgg2?  According to Table 5 in the HMC8410 data sheet, pin# 4 is NIC but Vgg2 is connected to pin# 4 shown in Figure 40 (evaluation board schematic) .

    1. pin# 4 is NIC and should be connected to RF/dc GND.
    2. pin# 4 is…
  • HMC8410 and inductor

    I have a question about HMC8410.
    Coilcraft 's 590nH inductor is used for the bias, but my customers say that this is not available.
    I must show customers how to choose an alternative inductor.

    I think L1 and L2 are choke coils.
    What is the performance…

  • HMC8410 Low Frequency Response

    The HMC8410 and 8410 evaluation board both list that the low-frequency cutoff is 10MHz when biased with the given bias network.  What is the low-end cutoff frequency of the SMT part and of the bare die without the bias network?  If I provide an extremely…