Do you have the reliability report for the HMC8400 amplifiers.
(specifically the HMC8402-die)
Hi HM,
Unfortunately, we do not have the 2nd & 3rd harmonic data for these parts (or the IP2 data required to calculate this) at the moment.
Thanks,
Dan
Hi avatar,
1) It's in series of the path.
2) I would recommend a bondable resistor from AVX.
3) The resistor in between the bypass capacitors is part of the noise filtering bypass circuit and also is there to protect the gate .
DanO
The largest temp range the DAC will operate per the data sheet is -40 to +85 C. If I get the die will it operate at -55 to 125C? I will be mounting the die on ceramic substrate.
does the assumption that it will work if properly heatsunk although the…
Please provide S-parameters for HMC939A-DIE. Thanks.
How can I determine the die temperature of your device?
Hi
Could you kindly let us know what difference with AD2428WCCSZ and AD2428WCCSZ01?
Our customer use AD2428WCCSZ01 first, but they want to modify to non-automotive version, but AD2428BCPZ no die revision, they confuse about it.
Where can I get the S parameter of LNA HMC341 measured on die? The S papameter offered on website is the results measured on test board.
Hello,
Do you have a maximum power consumption for the HMC598 in die form? The data sheet shows 175 mA @ 5 volts, but it's only a typical number and I'm seeing 220 mA @ 5volts, with no input signal or output load. Thanks.
Best Regards.
I wanted to Simulate the HMC392A in Microwave office. So i downloaded its S2P file from design resources and as i performed simulation its responses like return loss is better than the datasheet but its gain is decreased to max15.7 dB after simulation…