• HMC659-Die S-parameters

    Hello,

    Please share S-parameters of HMC659-Die.
    S-parameters of HMC659-Die cannot be found in ADI web site.

    Is using HMC659-Die with Vdd=5V Idd=100mA possible (recommended)?

    Best Regards,

  • AD9277 in die form?

    We would like to use AD9277 for a new design, an ultrasonic test equipment for
    material testing. High integration level and space saving are important aspects
    therefore the preferred component would be AD9277 in bare die (if available),
  • Die structure in OpAmps

    I would like to know what is the difference in the die structures of the following Op Amps

    • AD8620
    • AD8512
    • AD8513
    • OPA4227

    The main reason to know more about the die structures is to know how much the IC's will dissipate power supply current…

  • HMC451-die Drain modulaion

    Hi all,

    @ the datasheet HMC451-die, external bypass capacitors of 100 pF and 0.1 μF are required to Vdd1/Vdd2.

    Evaluating the HMC451-die for the Drain modulation, then the cap of  0.1 μF is large.

    Placing the both cap is recommended ?

    Replacing or…

  • HMC347A-Die v.s. HMC347B

    Hi all,

    Our customers have used HMC347.
    They will consider choosing a replacement product as the stock purchased at the last time buy will be gone.
    HMC347A-Die and HMC347B are both dies, and there is a difference between suffixes A and B.
    I do not know why…

  • Mixer in die form

    I am looking for a mixer with the following specs that is available in die form

    MIXER UpConverter

    Package DIE

    RF In Frequency

        2.0 to 5.94 GHz

    RF Out Frequency

        7.22 to 11.06 GHz

    LO Frequency

        13.15 GHz

    Conv Loss

        -7.5 dB

    ConvLoss Ripple

  • HMC505LP4 as naked die

    Dear Sir,

    Can we procude HMC505LP4 as naked die. We can afford a certain MOQ and NRE to do so.

  • ADA4870 Die Temperature Monitor

    Can I use the Thermal Monitor and Short-Circuit Flag (TFL) pin to monitor peak die temperature?

  • Questions for HMC902-Die

    Hello, I have a question from customer about HMC902-Die.

    In the Datasheet, the 100pF capacitors are mounted closed to Vdd and Vgg pin. Customer would like to know our recommended part for this. It is better to have the BOM for assembly diagram on page…

  • HMC641A-DIE datasheet specification

    Hi all,

    Could you please clarify  by the  datasheet for HMC641A-DIE.
    http://www.analog.com/media/en/technical-documentation/data-sheets/hmc641a.pdf

    The pads at the functional diagramm , outline drawing,  at the pad description table and assembly diagr…