• RE: FAQ: HMC8400 VG2 Voltage

    A: VG2 can safely be varied between 0V and -2V with VDD at 0V. However, VG2 should not exceed 0V when VDD is not present.

  • FAQ: HMC8400 Input

    Q: Is the RF input of HMC8400 actually ac-coupled?

  • HMC8400 AGC performance

    I am using the HMC8400 in a receiver design and I want to take advantage of its AGC capability by varying Vgg.  Do you have any data for the HMC8400 when Vgg is not left open?  Specifically, I would like to set the gain of the device near 0 dB.  What will…

  • LTC6268 Bare Die Pad Layout

    Hello,

    For a research project I am working on I need to use the LTC6268-10 op-amp. In my project I need to reduce the parasitic capacitance as much as possible. As a result, I am trying to get bare-die of this op-amp and directly wirebond it to another…

  • 2HD, 3HD data of HMC441-Die and HMC462-Die

    Hi, 

    Could you share the 2nd and the 3rd harmonic distortion data?

    If there is no data of these products, something of the same product series is also fine.

    Regards,

    HM

  • ltc2641 die -

    The largest temp range the DAC will operate per the data sheet is -40 to +85 C. If I get the die will it operate at -55 to 125C? I will be mounting the die on ceramic substrate.

    does the assumption that it will work if properly heatsunk although the…

  • HMC939A-DIE

    Please provide S-parameters for HMC939A-DIE. Thanks.

  • Die Temperature

    How can I determine the die temperature of your device?

  • HMC341 die

    Where can I get the S parameter of LNA HMC341 measured on die? The S papameter offered on website is the results measured on test board.