• RE: FAQ: HMC8400 Input

    A: The RF path is ac-coupled but there is a resistor to ground before the ac-coupling cap.

  • HMC8400 AGC performance

    I am using the HMC8400 in a receiver design and I want to take advantage of its AGC capability by varying Vgg.  Do you have any data for the HMC8400 when Vgg is not left open?  Specifically, I would like to set the gain of the device near 0 dB.  What will…

  • 2HD, 3HD data of HMC441-Die and HMC462-Die

    Hi, 

    Could you share the 2nd and the 3rd harmonic distortion data?

    If there is no data of these products, something of the same product series is also fine.

    Regards,

    HM

  • ltc2641 die -

    The largest temp range the DAC will operate per the data sheet is -40 to +85 C. If I get the die will it operate at -55 to 125C? I will be mounting the die on ceramic substrate.

    does the assumption that it will work if properly heatsunk although the…

  • HMC939A-DIE

    Please provide S-parameters for HMC939A-DIE. Thanks.

  • Die Temperature

    How can I determine the die temperature of your device?

  • HMC341 die

    Where can I get the S parameter of LNA HMC341 measured on die? The S papameter offered on website is the results measured on test board.

  • HMC598 Die

    Hello,

    Do you have a maximum power consumption for the HMC598 in die form? The data sheet shows 175 mA @ 5 volts, but it's only a typical number and I'm seeing  220 mA @ 5volts, with no input signal or output load. Thanks.

    Best Regards.

  • RE: HMC-ALH435-DIE 10 Ohms on Vgg1

    Hi avatar,

    1) It's in series of the path.

    2)  I would recommend a bondable resistor from AVX.

    3) The resistor in between the bypass capacitors is part of the noise filtering bypass circuit and also is there to protect the gate .

    Thanks,

    DanO

  • HMC392A-Die

    I wanted to Simulate the HMC392A in Microwave office. So i downloaded its S2P file from design resources and as i performed simulation its responses like return loss is better than the datasheet but its gain is decreased to max15.7 dB after simulation…