Besides the mismatch of the HMC836 bias network and values with the eval board, can it be the wrong(or inproper ) PLL Eval Software's settings that makes the output power weak?
Correction...
The HMC836 output component values should match the following and the eval board number is 125998-3. Use the "hmc836_Frac" eval board register configuration file.
R8=22
L4=1.5nH
L1=10nH
C8=8.2pF
C29=1.2pF
C31=not install…
想利用HMC836LP6CE产生一个3.5GHz的正弦信号,但是根据ADI上面的提供的USER-GUIDE操作时发现完全得不到正确信号,所产生的RF输出正弦波,不仅频率只有大概1.6GHz左右,而且Vpp大概只有15mV,而根据说明书上这个信号的典型值是6dbm,即便最低也有-1dbm,换算成Vpp的话大概是Vpp也有563mV。因此想请教一下有没有用过这款PLL的高手,指导一下。谢谢了!!!
Both HMC830 and HMC832 will meet these requirements but the application must utilize a tunable reference and manual tuning to meet the -60dBc spurious and hop time requirements. I've attached an appnote on manual tuning. With a fixed 50MHz reference Figure…
Hello,
I'm working with the PLL VCO HMC830.
I want to use a look-up table (LUT) for manual calibration, as decribe in "Frequency Hopping with Hittite PLLVCOs Application Note" (attached) (https : // www . hittite.com/content/documents/application_notes…
Use the ADP150 regulator; good performance, low cost.
Use…
This note discusses best practices for use of the Serial Port Interface (SPI) Mode selection feature of HMC PLL and PLLVCO product lines.
The attached FAQ document provides additional information on the use of the PLL+VCO and Clock Timing family of products. Specifically,
the applicable products are:
HMC820LP6CE HMC821LP6CE HMC822LP6CE HMC824LP6CE HMC826LP6CE
HMC828LP6CE HMC829LP6…