Why do the 16 feet (DVDD3V)have a 50 ohm resistance after 3.3V ?
有两个问题。
1,HMC830的DVDD3V脚,即16脚为什么要在加电3.3V后连一个50欧姆电阻。
Hello,
I have the Evaluation Kit for the HMC830LP6GE PLL with Integrated VCO and an external reference of 100 MHz. I'm running the the HMC PLL software version V3240.exe. The program appears to work fine, but when I tune to a frequency of 3GHz I…
Hello,
Would it be possible to get the Gerber files for the HMC830 Evaluation Board? We would like to use this as a known good layout for our board.
Best Regards.
Hi,
I have a problem with PLL HMC830.
I program HMC830 with parameters as follows :
Integer Mode for output = 50 Mhz (XTAL = 50 Mhz)
HMC830_HMC_Write(0, 0x20); // soft reset and = A7975 in read
delay (20);
HMC830_HMC_Write(1, 0x2);
HMC830_HMC_Write…
hi sir....
how to configure the register value for certain frequency values?...please tell me the procedure for to configure the register values.....
Hello,
Do you offer a Software Development Kit or sample code for "EKIT01-HMC830LP6GE" Fractional-N PLL with integrated
VCO with USB interface board.
Thanks.
Hello, I encounter a problem with the output voltage of HMC830 LD_SDO pin. The output voltage drops to 0.7V or 2.0v or other else between them after the device works for sometime. The output signal retains locked and eventhough the REG 0Fh is written…
I use 2x HMC830LP6GE on a radio design.
The Datasheet recommends to connect the N/C pins to Ground.
However, when I look at the schematics of your eval board, some of of the N/C pins are connected to VCC1 and other voltages.
I am on layout now and…