• RE: HMC829 spurious

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: HMC829 fails to start at high temperatures

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • HMC840 and HMC829 rapid frequency hopping

    We are using HMC840 and HMC829 devices, both with 100 MHz phase detection frequency (PDF). We need to perform frequency hopping (in a range of about 100 MHz) and do it as fast as possible (preferably less than 100 usec.).

    I have the following questions…

  • 关于hmc829的频率带宽问题

    在选型表中,hmc829的频率带宽有5.6-8.4Ghz,但在数据手册中却只有0.045至1.05, 1.4至2.1, 2.8至4.2,三种带宽,请问这是什么情况?

  • 请问hmc829或者830有没有寄存器编辑器?

    请问hmc829或者830有没有寄存器编辑器?

  • 求助,关于HMC829的几个问题

    应用情况:3.3V和5V供电,100MHz参考输入,100MHz鉴相频率,使其输出3.8GHz。环路滤波器与datasheet一致。由FPGA(EP3C5M164)对其进行寄存器配置。在调试中出现偶尔锁定输出,偶尔无输出的情况。

    问题如下:

    1.关于两个电源(3.3V和5V)的上电顺序,资料上说5V先加,或同时加。这个要求是否需严格执行?若3.3V先加,会有何后果?

    2.资料说必须先加上VDD后,才能加信号(参考)和SPI逻辑,以使进入想要的(HMC)模式。目前应用情况是,100MHz参考信号一直存在…

  • Is it possible to Frequency modulate the internal VCO of the HMC829 PLL?

    I would like to know if it would be possible to modulate in frequancy a closed loop with the HMC829 PLL. Actually what I want to know is if it would produce linear modulation response from the modulation input (good THD for audio modulating signals).

  • Hmc829 isolation between analog and digital inside the chip

    Hello,

    I'm using HMC829 RF PLL evaluation board I run the configuration from examples that Hittite provided,

    at the RF output I see some spurious at different places that running through small band =1MhZ when I click on read lock register(12h) with…

  • HMC829寄存器快速配置问题

    请问HMC830LP6GE寄存器快速编程指导是否适用于HMC829?

  • TAGS LIST: Clock and Timing

    LTC6953
    LTC6955
    LTC6957-1
    HMC6832
    HMC7043
    LTC6950
    LTC6954
    HMC987
    AD9576
    AD9508
    HMC1035
    HMC988
    HMC1033
    HMC1034
    HMC1032
    HMC1031
    ADN4670
    ADCLK944
    ADCLK950
    ADCLK948
    ADCLK846
    ADCLK954
    ADCLK946
    ADCLK854
    AD…