• HMC8205 - EVAL-HMC8205 Heat Sink

    Hello,

    I am interested in testing out the HMC8205 amplifier by first using the Evaluation board as a reference for later. I was wondering if there would be a need for an additional heat sink while using the HMC8205 Evalution Board at Psat (46 dBm). 

    Thank…

  • RE: HMC8205 - How to keep the conductivity between PCB and heatsink strongly?

    Hi,

          Solder is another alterative. Sheet solder 96.5 SN / 3.5AG. It comes in a sheet form. See attached photo.

    Regards,

    Jim B

  • PERFORMANCE OF POWER AMPLIFIER 35W HMC8205 EVM MODULE

    Hi,

    We tested HMC8205 power amplifier 35W, But we couldn't Get 35W power at Maximum Input RF power .

    We are driving with Driver Amplifier to HMC8205 in entire Band of Operation frequen.cy 400 to 6000MHz.

    Test Setup and Condition:

    Driver Amplifier…

  • [HMC8205] I wonder that HMC8205 can withstand how long, how much power at open/short load condition.

    We are thinking of using HMC8205 at under Psat(about 42 dBm).

    I wonder that HMC8205 can withstand how long, how much power at open/short load condition.

    In previous Q&As, ADI can not guarantee device survival under Open/Short Load at Psat power.

  • EVAL-HMC8205 P1 Pins

    Hi,

    I have purchased EVAL-HMC8205.

    Where can I find the pin information for the P1 connector that's on the board?

    Kind Regards.

  • FAQ: HMC8205 Reference Temperature

    Q: What is the reference when measuring temperature of HMC8205?

  • FAQ: HMC8205 NC Pins

    Q: Are the NC pins of HMC8205 true disconnects? Will there be issues connecting them to GND?

  • FAQ: HMC8205 Evaluation Board Connectors

    Q: What connectors are used for the HMC8205 Evaluation Board?

  • HMC980LP4E with HMC8205

    I would like to ask for advice. What to do for the VGATE of HMC980 to start at -4V and stop at -2.5V to raise the HMC8205 to meet the working conditions. Thank you.

  • Can HMC8205 be used at P1dB under open/short load condition

    My customer asked me the following questions.

    he wonder if IC be damaged or NOT.

    Would you answer them?

    1. Can HMC8205 be used at P1dB under open/short load condition?

    2. Can HMC8205 be used at P1dB and connect POUT with 90 degree hybrid coupler and…