• Application HMC8192 as frequency translator

    As the HMC8192 is  IQ passive mixer, is it a tru reciprocal device on all ports? I would like to use as frequency shifter . My input would be the LO port, I plan to drive the IF with a "quadrature DDS" and the output would be the RF port. I am expectin…

  • RE: IQ modulators and IQ demodulator (1GHz Baseband Bandwith)

    Hello,

    Please take a look at ADRF6780 IQ UC as a good example for integrated solution:

    http://www.analog.com/en/search.html?q=HMC8192

    as well as the HMC8191 for IQ passive mixer:

    http://www.analog.com/en/products/rf-microwave/mixers/iq-and-image-reject…

  • ADI 可用于 5G技术的资料大起底!

    Part 1:特色产品

    AD9164:16位、12 GSPS、RF DAC和直接数字频率合成器

    该DDS由一组32个32位数控振荡器(NCO)组成,各带相位累加器。与100 MHz串行外设接口(SPI)和快跳模式配合使用时,支持相位相干快速跳频(FFH)和几种模式以支持多种应用。

    http://www.analog.com/cn/products/digital-to-analog-converters/standard-dac/high-speed-da-converters/AD9164…

  • RE: “芯”来乍到,求赞、求围观!

    拾叁号芯品:宽带RF混频器HMC819x

    宽带无源同相正交RF混频器系列HMC819x,支持从2.5至42 GHz的完整频谱,与当今的其他分立式器件相比,它们提供了显著优势,为需要宽带支持的各种工业应用提供了理想解决方案,包括测试和测量等应用。

    要覆盖相同的频率范围,原先需要超过10个分立式器件,但ADI的这三款新器件就能实现这个目标,而性能没有丝毫影响。HMC819x混频器是业界唯一采用标准SMT封装的宽带解决方案,因而能够高效集成,缩短整体设计时间并降低风险,同时加快产品上市。

    了解该系列产品的详细产品介绍…

  • RE: ADI芯情2017大回顾,有奖认领属于你的“好芯事”

    两款宽带6 GHz模块HMC7885和HMC7748,最大程度地缩减子系统的尺寸和重量

    HMC7885和HMC7748宽带模块针对2 GHz至6 GHz频率范围的应用,包括测试和测量、通信、替代行波管(TWT)、航空监控、雷达等应用领域。这些完全集成的全固态器件扩展了ADI公司现有的GaN功率放大器系列,使用方便,可以加快原型开发和系统设计。

    产品详情:

    http://www.analog.com/cn/products/rf-microwave/rf-amplifiers/power-amplifiers…

  • 厉害了我的ADI,EDN Hot 100 占据16席!

    Hot 100 是 EDN 一项承传已久的历史活动,每年美国的编辑们都会选出当年最热门的100款产品分享给大家。

    2017 年最热的产品有哪些?EDN 编辑根据自己的判断和读者的兴趣选出了100个热门产品,其中 ADI 有 16 款产品上榜!手动鼓掌

    登上 EDN Hot 100 的 ADI 十六款产品都是哪些?它们为何如此受青睐呢,版主今天为你们说道说道~

    模拟器件:

    • LTC2358-18 SAR ADC

      LTC2358-18 是一款 18 位、低噪声、8 通道同时采样逐次逼近型寄存器 (SAR…

  • RE: 36GHz RF oscillation signal source

    You need a PLL which drives a frequency doubler which drives an amplifier. Possible choices might be ADF4371 (PLL),  HMC1105 (frequency doubler) and HMC7229 (amplifier). These are not the only choices.

      PDF

  • RE: Query

    This part is EAR99. The attached RFIC selection guide lists the ECCN codes for all of ADI's RF products.

     PDF