Could someone tell me what the video transient level is for the HMC802A attenuator? This is a measurement of the temporary voltage fluctuations that the device produces when it switches.
Hello,
We received question about switching noise of HMC802A from our customer.
According to the customer, he can see around 0.013mV switching noise at output pin of HMC802A when he changing to the attenuator. Is this value reasonable value for HMC802A…
I want to use RF switch HMC536 and RF attenuators HMC802, HMC629 for broadband application (LF...C-band). There is a requirement to use appropriate DC blocking capacitor in the datasheet on the RF input/output. Let assume that these parts are cascaded…
Hi,
Thank you very much for your reply.
I would like to have the power compression test data at 20MHz for HMC802A.
The 20MHz is our lowerst frequency.
Could you please provide the test data of power compression.
Best regerds,
Haru,
Hi All,
One of my customer made his prototype board with HMC802 mounted.
Three HMC802s are located at output terminal of his prototype and are connected in series.
He made 4 boards of prototype and 2 boards has problem.
The problem is very low impedance…
Q.
What are the differences between glitch free, safe state and no protection transitions in digital step attenuators (DSA)?
A.
Digital Step Attenuators usually have an array of attenuator stages internally and turning on or off the different stages…
RF和微波IC广泛用于电子测试和测量仪器,比如频谱分析仪、网络分析仪、信号发生器和通信测试仪。当无线通信在我们的生活中变得越来越普及,比如4G/5G和物联网,对于它们的测试基准的要求也在不断提高。在ADI针对电子测试和测量的RF和微波解决方案中,将重点讨论ADI产品如何融入相关信号链。
主要挑战和系统设计考虑
宽动态范围
最小化RF测试台的噪底(比如相位噪声)对于保持宽动态范围内的测试信号纯度很重要。但是,更多的数字信号处理任务将增加辐射噪声,因此获得干净的信号是个难题。
宽带宽