Hi All,
One of my customer made his prototype board with HMC802 mounted.
Three HMC802s are located at output terminal of his prototype and are connected in series.
He made 4 boards of prototype and 2 boards has problem.
The problem is very low impedance…
I am using 20dB attenuator(HMC802) which was working when tested earlier by feeding -30dBm power at 2250Mhz. Today, I tested again , the same power and frequency was given as earlier. In spectrum analyzer it shows -37dBm power. Even after changing the…
Hello All,
We would like to have the data of the HMC802's P0.1dB at lower frequency(DC - 100MHz).
As a datasheet at page3, There are not P0.1dB at DC -100MHz data.
We would like to have information of the P1dB around DC - 100MHz.
If you have information…
Hello,
I want to use RF switch HMC536 and RF attenuators HMC802, HMC629 for broadband application (LF...C-band). There is a requirement to use appropriate DC blocking capacitor in the datasheet on the RF input/output. Let assume that these parts are cascaded…