• HMC7992 DC blocking capacitors?

    The HMC7992 port specification says "...dc blocking capacitor is required on this pin". In our application we have three HMC7992 devices connected to each other. The inputs to the first HMC7992 that come from the signal source have DC blocking capacitors…

  • HMC7992 Frequency Range

    Hello,

    I'm little bit confusing about the frequency range of HMC7992. According to the datasheet, HMC7992 is Silicon SP4T Switch for 0.1GHz to 6.0GHA. But, we can see the following description in the General Description.

    "The HMC7992 has good low…

  • Where are the s-parameters for the HMC7992?  Do they extend beyond the freq specs of the device?

    I am looking for s-parameters for the HMC7992 SP4T RF Switch.  Do they extend beyond the 100MHz to 6GHz specified range for the part? 

  • RE: design files for EV1HMC7992LP3D evaluation kit

    Hello Ales, 

    You can find the schematic in the attachment below. 

    In addition, BOM can be seen on datasheet page 11/12 of HMC7992. 
    www.analog.com/.../HMC7992.pdf

     PDF

  • RE: UHF RFID 902MHz-928MHz antenna switch sp4t

    Thank you EricC,

    I chose the HMC7992 ic, It's working ok.

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225
  • 11/18/15: RF & MW Control Products in Silicon

    Presenter: Bilge Bayrakci

     

    In this webcast, we will introduce Analog Devices' new RF & MW switch and attenuator family of products implemented in advanced silicon process. We will discuss how the new products benefit from the inherent advantages of…

  • 【在线研讨会讲义PPT下载】采用硅技术的射频和微波控制产品,你了解吗?

    砷化镓技术是射频和微波器件设计的常用技术,但如果产品要求快速建立时间和快速开关时间,硅工艺优于砷化镓。

     

    那么问题来了——

    采用硅技术的射频和微波控制产品,相比砷化镓器件,优势在哪里呢?

     

    为此,ADI举行了一场主题为【采用硅技术的射频和微波控制产品】的在线研讨会。在研讨会中,ADI射频和微波控制产品部门营销经理Bilge Bayrakci 介绍了ADI采用先进硅工艺制造的新型射频和微波开关以及衰减器系列产品。相比使用砷化镓制造的传统计数器件,Bilge 讨论了新产品如何从硅技术的固有优势中受益…

  • RE: Query

    This part is EAR99. The attached RFIC selection guide lists the ECCN codes for all of ADI's RF products.

     PDF

  • RE: 36GHz RF oscillation signal source

    You need a PLL which drives a frequency doubler which drives an amplifier. Possible choices might be ADF4371 (PLL),  HMC1105 (frequency doubler) and HMC7229 (amplifier). These are not the only choices.

      PDF