Can you provide S-Parameters for HMC7891?
Since the goal is frequency demodulation, what is the AMPM/AMFM performance of the HMC7891?
On behalf of John Wise.As a general response, if the limiting amplifier output was fed into an RF detector the detected voltage would be proportional to the RF output power of the HMC7891. If the off pulse is below limiting and the on pulse is within…
On behalf of John Wise.
For the HMC7891 it is recommended that the input power does not exceed 15dBm. This is based upon the design of the amplifier which accounts for the maximum input drive at each amplifier stage.
On behalf of John Wise.The answer depends on the frequency offset of the two tones, the expected output would be at the limited output and the difference would be very small. If the frequency separation is wide, then the difference in amplitude would be…
弹指一挥,2016年所剩时间已不多咯,快到年底啦~
截至到今天,ADI在2016年发布了19款产品,产品包括了放大器、数据转换器、数字隔离器、电源管理、微控制器、射频收发器……这里,坛主将带领大家一起回顾下这些新品,其中不乏将影响未来电子技术应用趋势的大牛产品哦~
作为一枚工程师,对每一款与你工作紧密相关的新品,你一定细致阅读其每一个关键指标参数,每一丝改善你一定会从内心欣喜,对么?
so,对我们的19款新品,哪款最让你动芯?
欢迎跟帖,当一回评委,选出你最动芯的ADI新品——选择条件…