Hi,
What is the status of HMC717A? Maybe you have any information about leaving pre-release stage?
Best regards,
Pawel
Dear Supporter
I need a replacement for the HMC604LP3E with its By pass feature.
From ADI's web site, the HMC717A Low Noise Amplifier SMT, 4.8 - 6.0 GHz is proposed as alternative but witout by-pass.
Any advise on other alternatives?
Thanks
Hi Anton*89,
Yes, the two cascaded gain stages could oscillate if the oscillatory criterion are met. To minimize the chances of that happening, I recommend that you try to maintain a good match between all RF ports to minimize reflections and maintain…
好久木有推荐产品了,今天安利5款ADI正在重点推广的产品,包括ADC、放大器、收发器……如果您的设计中需要它们,可点击相关链接申请样片或购买产品,若在使用中遇到问题可在本社区发布帖子进行提问,咱们有工程师为您解答哦
NO.1:SAR ADC AD4000
AD4000是一款低噪声、低功耗、高速、16位、2 MSPS精密逐次逼近型寄存器(SAR) ADC,它集成了易用特性,可降低信号链的功耗和复杂性,支持较高的通道密度。高阻态模式与长采集阶段的结合,无需使用专用的高功耗、高速ADC驱动器即可扩展直接驱动此ADC的低功耗精密放大器的范围…