• HMC702 Reg Map

    ADI if can provide HMC702 Register configuration guide file?

  • HMC702 grounding

    The HMC702 PLL is a mixed analog/digital part with numerous grounds.  Should all the grounds be tied together to a single ground or should the analog and digital ground planes be kept separate and tied together using an inductor?

  • Questions about HMC702

    Hi,

    I have two questions about HMC702.

    1. Let me know the following spec of trigger signals to start sweep modes.

             Minimum pulse width, Low/High level threshold voltage

    2. Please take a look at the attachment. I have a question about the sweep_busy…

  • HMC702锁定检测

    目前寄存器设置如下:

    Reg 01h<14> = 1

    Reg 1Ah<9:0> = 40h ;     Reg 1Ah<11:10> = 1:1 ;     Reg 1Ah<13:12> = 1:0 (我在这里把LD—SDO接口强制设置在锁定检测状态,不需要其进行SDO串行数据输出);    Reg 1Ah<19:14> = 0h ;

    Reg 1Bh<3:0> = 2h ;

    按照以上设置,我用频谱仪检测到输出信号已经锁定后,LD-SDO接口始终没有输出一个高电平…

  • HMC702 and ADF5356?

    Hi, 

    I was wondering if the HMC702 and ADF5356 are compatible with each other? Can the ADF5356 be used as a VCO for HMC702 to sweep the entire band?

    Regards,

    Amin

  • RE: Noisefloor degradation of HMC702 Sweep Mode

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: HMC702 HMC703 HMC704  Phase Noise of Reference Oscillators

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • HMC702 current of 3.3V

    I'm thinking of using HMC702 and HMC1060 to build a phase lock loop.HMC702 is a quite great frequency synthesizer IC and HMC1060 is a LDO which can produce one 5V 300mA,two 3.3V 50mA and one 3.3V 100mA in one IC.In HMC702's datasheet ,it says that +3…

  • hmc702+hmc582

    eval-hmc702lp6c,开发板,是否能够实现10-12GHz的扫频,在少于1秒的时间内。

  • HMC702 Lock Issue

    Hi,

    I have made a chirp signal generator which should sweep from 10GHz to 14GHz based on HMC733 and HMC702. The schematic of HMC702 evaluation board was used as a reference. My issue is the board can only lock at the frequency band higher than 11GHz…