Hi,
I would like to know how HMC694 VGA control port influences at RF ports and vise versa. There is no any data in the datasheet.
Would it be possible to provide here isolation between Vctrl and RFin/RFout as well as between RFin/RFout - Vctrl?
Regards…
Hello,
Do you have data of P1dB vs. CTRL? I can find data of NF vs. CTRL and P1dB vs. Temperature. But I can't find the data of P1dB vs. CTRL in the datasheet of HMC694. I would like to get P1dB vs. CTRL for 9GHz to 10GHz.
Best regards,
Akira
Hi HM,
Unfortunately, we do not have the 2nd & 3rd harmonic data for these parts (or the IP2 data required to calculate this) at the moment.
Thanks,
Dan
Is there anyone can help with this?
Appreciate.
The largest temp range the DAC will operate per the data sheet is -40 to +85 C. If I get the die will it operate at -55 to 125C? I will be mounting the die on ceramic substrate.
does the assumption that it will work if properly heatsunk although the…
Please provide S-parameters for HMC939A-DIE. Thanks.
How can I determine the die temperature of your device?
Hi
Could you kindly let us know what difference with AD2428WCCSZ and AD2428WCCSZ01?
Our customer use AD2428WCCSZ01 first, but they want to modify to non-automotive version, but AD2428BCPZ no die revision, they confuse about it.
Where can I get the S parameter of LNA HMC341 measured on die? The S papameter offered on website is the results measured on test board.
Do you have a maximum power consumption for the HMC598 in die form? The data sheet shows 175 mA @ 5 volts, but it's only a typical number and I'm seeing 220 mA @ 5volts, with no input signal or output load. Thanks.
Best Regards.