• HMC675LC3C - Track Mode & Analog Comparator

    Hi,

    I used a HMC675LC3C as Analog Comparator High Speed.

    The input INP receive an adjustable DC  signal  (0V to -0.75V) and the input INN  a burst of negatives pulses . Pulses are 600ps width.

    I would compare these 2 signals to obtain an output signal.

  • RE: HMC675LC3C VCCO and VEE

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: As for holes on the EVB of HMC675LC3C

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • COnfusion about LE pins of HMC675LC3C

    Hello,

       I need help regarding HMC675LC3C. I have a confusion.

     

    I need to give clock at 8.9 GHz at LE pin.In latch enable characteristics, Latch Enable Input Range is from 1.6V to 2.4V. What does this mean? Is this Voh value ? i.e if voltage is between…

  • HMC675LC3C技术手册中的最小脉冲宽度是指什么?

    现在计划用这款比较器去对重复频率为10GHz的脉冲信号进行整形,在芯片的输入端一端输入脉冲信号,另一端为固定电压信号,当脉冲信号电压比固定电压信号电压高的时候,输出为1,比固定电压信号电压低的时候输出为0。不知道这么用可以吗?

    芯片手册中提到了最小脉冲宽度,不知道是指什么?是指输入信号的最小脉冲宽度吗?

  • RE: LMH7322 pulse stretch

    Hi drachir_1900,

    The sub nanosecond prop delay comparators are mostly characterized with IBIS models. Here is a list of devices from ADI for your reference:

     XLSX

    Regards,

    Hooman