• HMC1061 and HMC661 thermal resistance

    Hi,

    Can you provide the junction-to-case thermal resistance (both top and bottom) of HMC661 and HMC1061?

    Thank you.

  • RE: Configuring phase relationship between two outputs of HMC7044 with Analog fine delay feature

    Thank you! Nice answer! Many datasheets say that analog delay may cause some phase noise degradation. Do anyone know how much is this degradation? how much will it increase jitter? In my application i want to clock track and hold amplifier hmc661 with…

  • RE: 关于采样保持板HMC661LC4B

    可以购买ADI的HMC9000进行测试,HMC9000包含HMC661和ADC芯片,可以直接测量。

  • T&H IC Sampling Speed for HMC5831

    Dear Sir,

    I have one more question.

    HMC5831 provides 26 G-sampling per sec operation,

    however, I can’t find the ultra-high speed T&H IC that can support 25G-sampling per sec on HMC5831.

    The fastest I have found is HMC661 or HMC5640 that specifies…

  • RE: Clock frequency of HMC661LC4B

    The HMC661 device has minimum clock frequency of 250MHz as specified in the datasheet. If you clock it at a lower frequency, and 50MHz is lot lower than 250MHz, the droop will be too severe and some datasheet performance specs will be violated. So we…

  • 3月重点推荐——民用雷达解决方案,是你的菜么?

    雷达广泛用于民用应用,从执法部门实施的汽车系统和速度监控到空中交通管制、天气和海上监控。雷达发射无线电波,然后通过其路径中的物体反射。雷达接收机处理这些反射波以确定物体的范围、角度或速度。例如,海上雷达可测量船舶方位和距离以防碰撞并进行船舶导航。在港口或海湾处,船舶交通服务雷达系统用于监控和调节繁忙水域中的船舶运动。配合飞机应答机系统一起使用的类似民用空中交通管制雷达确定相似特性,以确保飞机之间保持安全距离并协调飞行路径。

    主要挑战和系统设计考虑

    远程监控雷达,如空中交通管制、天气和海上雷达…

  • Wright Brothers Appreciation Day

    In anticipation of Wright Brothers Appreciation Day, we reached out to a few of our engineers who also log time flying the fair skies. Here’s what they had to say about aviation, ADI, and the legacy of the Wright Brothers.




    Brad Hanson

  • RE: Query

    This part is EAR99. The attached RFIC selection guide lists the ECCN codes for all of ADI's RF products.

     PDF

  • RE: 36GHz RF oscillation signal source

    You need a PLL which drives a frequency doubler which drives an amplifier. Possible choices might be ADF4371 (PLL),  HMC1105 (frequency doubler) and HMC7229 (amplifier). These are not the only choices.

      PDF