• How to measure AD7606C die temperature with the diagnostic multiplexer?

    Each of the eight channels has a diagnostic multiplexer in front. So, it can be enabled in order to monitor an internal node instead of the analog input signal (Vx+ - Vx-).

    This can be enabled, when in software mode and +/-10V selected, by accessing the…

  • 2HD, 3HD data of HMC441-Die and HMC462-Die

    Hi, 

    Could you share the 2nd and the 3rd harmonic distortion data?

    If there is no data of these products, something of the same product series is also fine.

    Regards,

    HM

  • AD777x: How can the temperature of the die be calculated?

    In the datasheet the equation to calculate the temperature can be found.
    This equation calculates the temperature rise referred to 25°C, so to calculate the absolute temperature it is necessary to add 25° to the previous equation:
    The DVbe voltage…
  • RE: Pluto SDR in Ethernet Adaptor Mode Randomly Has Adaptor Die

    I know some people reported USB disconnect issues before.

    If you google for "PlutoSDR GND modification" you will find some.

    This one for example: http://oe7wpa.com/index.php/projekte/elektronik/datv/qo-100-mit-dem-adalm-pluto/qo-100-datv-betrieb…

  • RE: HMC985A-Die rf pins interchangeability

    Hi,

    HMC985A-Die can support bi-directional operation, however, the power handling for RFOUT might be lower than RFIN.

    The absolute max RF input power for HMC985A-Die is 30dBm as listed in the datasheet, therefore, I think it is OK to apply 15dBm max to…

  • LTC6268 Bare Die Pad Layout

    Hello,

    For a research project I am working on I need to use the LTC6268-10 op-amp. In my project I need to reduce the parasitic capacitance as much as possible. As a result, I am trying to get bare-die of this op-amp and directly wirebond it to another…

  • RE: HMC658

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • Can I get a packaged fibre optic transimpedance amplifier from ADI (not in die form)?

    Is it possible to get transimpedance amplifiers in a SOP package? Looks like
    only dice is provided by ADI?

     

    AD8015, 155 Mbps Transimpedance Amplifier is available in 8 lead SOIC package
    or in die form. The other Transimpedance Amplifiers are…

  • LT1764ADICE and LT1175-5DICE Die Composition and Bond Pad Metallization

    Hello,

    Please provide LT1764ADICE and LT1175-5DICE Die Composition and Bond Pad Metallization. I am unable to locate this information.

    Thank you in advance,

    StoneOLD