• Will you provide in Die ? so that we can integrate on our SOIC

  • OP293: Available as bare die

    I require an op-amp with a fairly basic electrical spec but it must be
    available in die form for incorporation onto a microwave substrate in a sealed
    module.  It must operate from a single +5v supply and the input voltage range
    should extend down…

  • Aol G differences OpAmp to Opamp on same die, same for BW

    In parts that have multiples of OpAmps on the same die, in the same package, what can one expect

    the Aol and BW differences will be one OpAmp to another ? In rough percentages.....?

    Regards, Dana.

  • Information about REF43NBC Die part

    Is the Lifecycle status for Die part “(REF-43(1802Y)” and the REF43NBC the same?

    Can you please give me the lifecycle status for REF-43(1802Y.

     

    1802Y is the dice’s mask set ID and the part that customers can order is the
    REF43NBC…

  • AD825 die X-Y coordinate

    What is the size of the die in X-Y coordinate?

     

    See attachment.
    Attachments:
  • 2HD, 3HD data of HMC441-Die and HMC462-Die

    Hi, 

    Could you share the 2nd and the 3rd harmonic distortion data?

    If there is no data of these products, something of the same product series is also fine.

    Regards,

    HM

  • ADMV8818 in die form?

    Hi,

    Is ADMV8818 available in die form? Or is there any plan to launch it as a die product? 

    Thank you in advance!

  • HMC985 die

    Does anybody know why the HMC985 die has metalization on the edge?

    Thanks.

  • AD825 die co-ordinate info detail request

    I am using die components on a MCM. I would like to have information on pads
    location (X-Y coordinates) and back side connection. Could I have this document?
    Document is a die description.

     

    These are dedicated and proprietary info which…
  • How to measure AD7606C die temperature with the diagnostic multiplexer?

    Each of the eight channels has a diagnostic multiplexer in front. So, it can be enabled in order to monitor an internal node instead of the analog input signal (Vx+ - Vx-).

    This can be enabled, when in software mode and +/-10V selected, by accessing the…