• HMC347B and HMC641A Bond Pad Metallization

    Hello,

    Can you please provide the Bond Pad Metallization for HMC347B and HMC641A Die? I cannot locate this information in the Datasheets.

    Thanks in advance,

    StoneOLD

  • RE: HMC641A-DIE datasheet specification

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADRF5424 Die Form

    Hi,

    Is ADRF5424 available in die form?

    What does Die on Carrier means?

    Thank you.

  • HMC797A-Die

    Hi,

    Is it possible to maintain RF ON while the amplifer is OFF?

    Thank you so much

    Chiara

  • ADRF5044 DIE

    Is this product available in DIE form?

    Thanks

  • ADPA 7008 and ADPA 7009 die attachment

    We would like verify the die attachment method for ADPA 7008 & 7009 is epoxy.

    Is there anything in particular we need to use? Any brand suggestions or recommendations?

  • HMC-ABH241 : Die Related- Queries

    Find both Q&A below. 

     

    1. We only show decoupling for one side of the die. The top side in the view
    below has the same supply pads. Is decoupling only on one side required and can
    it be either side?
    Yes the supplies only on south or north side can…

  • DIE level parts?

  • RE: HMC641ALC4 vs ALP4 vs A-DIE frequency range ?

    Hi sss,

    Unfortunately, the lower frequency on the older HMC datasheets were incorrectly specified.
    We are correcting this as we convert the datasheet to the ADI-format.

    We have converted the HMC641A-DIE and the -ALP4 datasheet already, and will convert…

  • ADL6010 bare die temperature range

    The packaged variants of the ADL6010 comparator include devices that are rated for a -55C to +125C temperature range.  There is also a space qualified version of this device (ADL6010s-DIE) that is rated for -55C to +125C.  I need a die part with a -55C…