• HMC602 - Rise Time and Fall Time

    Hi, I'm measuring the rise and fall time of the HMC602 with an input power changing between -60dBm and -20dBm and I'm getting values much biffer than the ones stated in the datasheet (In the order of 700us). Can you please provide me the way the rise…

  • HMC602 Succeptability to radiated RF

    Using the HMC602 as a detector in a RX AGC loop. The HMC602 is detecting the Tx signal (possibly radiated) at higher levels that the RX (conducted) signal. The RX path and AGC circuit is on the bottom side of the board and Tx is on the top side. Has anyone…

  • HMC602LP4E and HMC346AMS8GE for ALC

    Hi,

    Can you provide some application note regarding the controller mode of the HMC602 (or equivalent log detector/controller) ? We recently acquired evaluation boards for the HMC602LP4E and HMC346AMS8GE in order to implement an analog ALC loop in an experiment…

  • ADRF6720 VPTAT output characteristics ?

    Hello, 

    What's the characteristics (coefficients, precision) of the VPTAT output of the ADRF6720 ?

    I find some information about VPTAT but nothing really coherent :

    ADRF6720 temperature breakdown

    TMP01 tolerance calculation 

    HMC602 & HMC611 Temp…

  • RE: HMC602LP4E - "TEMP" pin

    It will probably the same or very similar to the HMC611 temp sensor output (see below).

    I will try to find the HMC602 temp sensor output plot.

    Update:  The HMC602 has the same slope and intercept as the HMC611 on its TEMP pin.

  • 超高频包络检波选型咨询

    现在有几款检波器分别是HMC602,ADL5513,ADL5511,HMC1120,哪一款适合300MHZ—1.5GHz包络检波

  • ADI针对电子测试和测量的RF和微波解决方案,优势在哪?

    RF和微波IC广泛用于电子测试和测量仪器,比如频谱分析仪、网络分析仪、信号发生器和通信测试仪。当无线通信在我们的生活中变得越来越普及,比如4G/5G和物联网,对于它们的测试基准的要求也在不断提高。在ADI针对电子测试和测量的RF和微波解决方案中,重点讨论ADI产品如何融入相关信号链。

    主要挑战和系统设计考虑


    宽动态范围

    最小化RF测试台的噪底(比如相位噪声)对于保持宽动态范围内的测试信号纯度很重要。但是,更多的数字信号处理任务将增加辐射噪声,因此获得干净的信号是个难题。

    宽带宽

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…
  • 12/16/2015: Full RF Signal Chains from 0Hz to 110GHz

    Presenter: Mel Conway, Product Manager, Instrumentation, High-speed & RF and Precision

     

    This webcast will explain ADI's new and expanded RF capabilities since the acquisition Hittite Microwave. We will give examples of the wider frequency spectrum…

  • 【在线研讨会讲义PPT下载】从0Hz到110GHz的全频谱RF信号链

    此次在线研讨会阐释了自收购Hittite Microwave后ADI的全新及扩展的RF能力。我们会举例说明ADI涵盖的更宽频谱范围及其真DC的重要性。信号链外的性能同样至关重要,展示低噪声、高稳定性控制和电源元件如何改善总体RF信号性能,并将讨论完整的信号链示例。

    主要讨论天线到比特和比特到天线,信号链覆盖,即刚才提到的从真正的DC 0 Hz到110 GHz的频谱覆盖。 我会简要介绍其中涉及到的各类设备。

    为什么良好的RF需要良好的电源,大家知道,RF需要干净的电源。然后,最后会和大家讨论“不止是芯片…