• HMC595A hot switching, max power?

    I have an application where I have to switch a 200MHz 34dBm CW signal. Switching rates will be low, about 1KHz.

    The HMC595A seemed like a fine option, however I don't see a 'hot switching' spec in the datasheet.

    I would like to know if it…

  • HMC595A/HMC574A transients

    What is the video transient/feed-through for the following RF switches.

    HMC595A
    HMC574A

  • RE: HMC595AE_Tj

    Hi,

    HMC595A is specified to have thermal resistance of 109 C/W from junction to die bottom and maximum junction temperature rating of 150 C. 

    Best.

  • RF Switch Logic


    I want to confirm the logic of RF switch of models below:

    HMC595A

    HMC545A

    The truth table for them on RF1 & RF2 against A & B are reverse? can not direct replacement? Please advise.

  • RF switch logic

    Dear  Sir/Madam

    I want to confirm the logic of RF switch of models below:

    HMC595A

    HMC545A

    The truth table for them on RF1 & RF2 against A & B are reverse? can not direct replacement? Please advise.

    Thanks.

  • RE: HMC784MS8GE not recommended for new designs?

    FormerMember
    FormerMember

    Hi,

    The HMC784MS8GE is not recommended for new designs because it will be discontinued. A PDN on EOL will be issued in June'2016 with LTB order dated Dec'2016.

    We will have a replacement for the HMC784MS8GE. The HMC784AMS8GE will be the FFF…

  • RE: HMC595E

    FormerMember
    FormerMember

    Hi,


    It may be helpful to have a bit more information on measurement conditions and test setup.

    Do you evaluate the HMC595E on its eval board? If not, did you confirm by thru measurement or simulation that the transmission lines on your PCB have 50ohm…

  • 总有一款适合您——最新《RF和微波IC选型指南》PDF免费下载ing

    天线到数字以及数字到天线……ADI凭借领先的射频技术能力、系统知识与工艺技术,提供直流到90 GHz以上、涵盖整个RF信号链最丰富多样的RF IC组合。

     

    面对上千款的RF IC产品,如何选出最适合自己应用的哪一款呢?ADIRF和微波IC》最新选型指南来帮您。(附件)

     

    最新版的《RF和微波IC》选型指南主要包括RF放大器、可变增益放大器、衰减器、RF混频器、I/Q调制器和解调器、集成式收发器……


  • RE: Query

    This part is EAR99. The attached RFIC selection guide lists the ECCN codes for all of ADI's RF products.

     PDF

  • RE: 36GHz RF oscillation signal source

    You need a PLL which drives a frequency doubler which drives an amplifier. Possible choices might be ADF4371 (PLL),  HMC1105 (frequency doubler) and HMC7229 (amplifier). These are not the only choices.

      PDF