• HMC575 in an Upconverter

    Hello,

    I am trying to design an RF upconverter using HMC575.

    Would it be possible to use one of the transmitters like ADRV9008-2, and connect it directly to HMC575 to work in the X-band? I was also wondering what would happen if we input modulated signals…

  • RE: Residual phase noise of HMC575 and HMC573

    Absolute Phase Noise Plots for HMC573 and HMC575.  These include the phase noise from the signal generator.  Signal generator was set to 4.5GHz.  Both parts phase noise at 9GHz.  If the input signal source is limitting the phase noise, the 9GHz output should…

  • HMC575 input power to output power does not conform to the datasheet!

    Hi there,

    I am using the HMC575 evaluation board and I am trying to validate HMC575 for our design. I have a 3 Ghz signal coming in (from a signal generator) and I put that signal through a band pass filter (2.7GHz to 3.1GHz) to clean any extra spurs…

  • What happens to the HMC575 when no input signal is present? 

    50 Ohms termination to ground on input.  Will it self-oscillate?

  • TAGS LIST: RF and Microwave

    HMC928
    HMC929
    HMC931
    HMC932
    HMC933
    HMC934
    HMC935
    HMC247G
    HMC538
    HMC-C018G
    HMC-C025G
    HMC-C053G
    HMC-C584G
    HMC7056G
    HMC7054G
    HMC7053G
    HMC7056AG
    HMC642G
    HMC642AG
    HMC643G
    HMC644AG
    HMC647
    HMC647A