• Propagation delay for HMC574A

    Hi, I would like to use HMC574A.

    So, I have a question. Please help me.

    Question:

    Can you tell me the propagation delay of the HMC574A?

    I am trying to switch high frequency signals using the HMC574A.
    The signal frequency is about DC to 30MHz, and the…

  • HMC595A/HMC574A transients

    What is the video transient/feed-through for the following RF switches.

    HMC595A
    HMC574A

  • Please tell me about the operation of HMC574A.

    Hi, I would like to use HMC574A.

    So, I have a question. Please help me.

    Question:

    I am experimenting with an evaluation board.

    The A and B terminals of the HMC 574A, 
    I think that the logic level needs to be different at every timing.
    First of all is this…

  • I want a board pattern diagram / layout about the HMC 574A evaluation board

    Hi, I would like to use HMC574A.

    So, I have a question. Please help me.

    Question:

    I use an experiment with the HMC574A evaluation board.

    There is a restriction on the size of the device and the evaluation board can not be entered as it is.

  • Suggestions for +8V logic to drive HMC574AMS8E?

    Hi,

    I would like to run the the HMC574AMS8E at Vdd=8V for the higher P0.1dB.  The HMC574AMS8E datasheet shows a schematic (pg. 6) where the Vdd of the HMC574A and the 74HC04 logic share the same +Vdd.  Note 2 (also pg. 6)  says:

    "Control inputs A/B can be…

  • HMC574AMS8E Hot Switching?

    I'm looking at the HMC574A part, however I don't see any mention in the datasheet about "hot switching". In my search of comparable parts there seems to be stated limitations to the performance when switching an always on maximum power RF…

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225
  • how to slow down ADG714 switch timing

    Hi,

    I am using ADG714. One side of the switch is connected to an amplifier set at 1000X gain. When I close the switch, I see a spike at the output of the amplifier. I suspect that is because the switch is closed too fast and I need to slow down the switch…