• HMC565

    Hello,

    Could you please verify that the S-param files for the HMC565 Die are correct, and if they will work with Agilent Genesys 2012. I'm unable to import the s-parameter data into Agilent Genesys 2012 and This is the only file I've had trouble with…

  • HMC565 Max RF Input Power

    With the HMC565 datasheet, is the absolute maximum ratings on page 6 for the RF Input Power correct?  The maximum input power is +0dBm?

  • HMC997 and HMC565 Demo-board Capacitors

    Hello,

    I am experiencing some differences between my PCB's (replicas of the demo boards) using these integrated circuits and the demo board that I ordered from Hittite. As these differences are the same and occur on the same bands (approx 17 GHz) in…

  • RE: 2HD, 3HD data of HMC441-Die and HMC462-Die

    Hi HM,

    Unfortunately, we do not have the 2nd & 3rd harmonic data for these parts (or the IP2 data required to calculate this) at the moment.

    Thanks,

    Dan

  • Can HMC565 and HMC997 have their supplies switched dynamically to switch transmission and reception paths?

    Hi,

    We have a loop made of these two amplifiers. However, they are on diferent paths isolated with RF swtiches. These switches are not sufficient to grant isolation though. For this reason an oscillation occurs at around 22 GHz. To compensate this, we…

  • AD2428WCCSZxx die revision

    Hi

    Could you kindly let us know what difference with AD2428WCCSZ and AD2428WCCSZ01?

    Our customer use AD2428WCCSZ01 first, but they want to modify to non-automotive version, but AD2428BCPZ no die revision, they confuse about it.

  • ltc2641 die -

    The largest temp range the DAC will operate per the data sheet is -40 to +85 C. If I get the die will it operate at -55 to 125C? I will be mounting the die on ceramic substrate.

    does the assumption that it will work if properly heatsunk although the…

  • HMC939A-DIE

    Please provide S-parameters for HMC939A-DIE. Thanks.

  • Die Temperature

    How can I determine the die temperature of your device?

  • HMC341 die

    Where can I get the S parameter of LNA HMC341 measured on die? The S papameter offered on website is the results measured on test board.