• 2HD, 3HD data of HMC441-Die and HMC462-Die

    Hi, 

    Could you share the 2nd and the 3rd harmonic distortion data?

    If there is no data of these products, something of the same product series is also fine.

    Regards,

    HM

  • RE: HMC985A-Die rf pins interchangeability

    Hi,

    HMC985A-Die can support bi-directional operation, however, the power handling for RFOUT might be lower than RFIN.

    The absolute max RF input power for HMC985A-Die is 30dBm as listed in the datasheet, therefore, I think it is OK to apply 15dBm max to…

  • HMC985 die

    Does anybody know why the HMC985 die has metalization on the edge?

    Thanks.

  • RE: LTC6268 Bare Die Pad Layout

    Hi Alex:  If you send me a photo of the die, I can mark it up with the bond pad names.  Please email me at glen.brisebois@analog.com

  • ltc2641 die -

    The largest temp range the DAC will operate per the data sheet is -40 to +85 C. If I get the die will it operate at -55 to 125C? I will be mounting the die on ceramic substrate.

    does the assumption that it will work if properly heatsunk although the…

  • HMC939A-DIE

    Please provide S-parameters for HMC939A-DIE. Thanks.

  • Die Temperature

    How can I determine the die temperature of your device?

  • HMC341 die

    Where can I get the S parameter of LNA HMC341 measured on die? The S papameter offered on website is the results measured on test board.

  • HMC598 Die

    Hello,

    Do you have a maximum power consumption for the HMC598 in die form? The data sheet shows 175 mA @ 5 volts, but it's only a typical number and I'm seeing  220 mA @ 5volts, with no input signal or output load. Thanks.

    Best Regards.