• HMC341 die

    Where can I get the S parameter of LNA HMC341 measured on die? The S papameter offered on website is the results measured on test board.

  • Die Temperature

    How can I determine the die temperature of your device?

  • ltc2641 die -

    The largest temp range the DAC will operate per the data sheet is -40 to +85 C. If I get the die will it operate at -55 to 125C? I will be mounting the die on ceramic substrate.

    does the assumption that it will work if properly heatsunk although the…

  • HMC392A-Die

    I wanted to Simulate the HMC392A in Microwave office. So i downloaded its S2P file from design resources and as i performed simulation its responses like return loss is better than the datasheet but its gain is decreased to max15.7 dB after simulation…

  • HMC598 Die

    Hello,

    Do you have a maximum power consumption for the HMC598 in die form? The data sheet shows 175 mA @ 5 volts, but it's only a typical number and I'm seeing  220 mA @ 5volts, with no input signal or output load. Thanks.

    Best Regards.

  • HMC939A-DIE

    Please provide S-parameters for HMC939A-DIE. Thanks.

  • RE: AD8354 bare die

    It's only available in bare die. Below are some alternative devices available in die form that cover the same frequency range.

    HMC395 Gain block 0 to 4000
    HMC397 Gain block 0 to 10,000
    HMC405 Gain block 0 to 10,000
    HMC396 Gain block 0 to…
  • RE: HMC129 part compatibility 1997rev and a 2007 rev part

    Hi,

    Firstly if the HMC129 is going to be used for a new design then please be aware that this part is not recommended for new designs.

    The 2 die are different due to a process change. The performance between the 2 die should be similar (isolation).…

  • RE: C band power amplifier

    A die is just a small piece of semiconductor material on which an integrated circuit has been fabricated and cut from a semiconductor wafer. You would not be able to solder a die to a PCB and make direct contact with the signal pads. You would instead…

  • Packaged Part Numbers

    Are these the correct packaged part numbers for the following die products?
    HMC913-Die = HMC913LC4B
    HMC907A-Die = HMC907APM5E

    If so, where can I locate the schematics for following evaluation boards?
    EVAL-HMC913LC4B
    EVAL-HMC907APM5