• RE: HMC554 S-Parameters

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: HMC554 : Not Recommended for New Designs ?

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • In my application, I want to use hmc554 in upconversion mode. Input LO is 13-18 GHz with the power of -2 dBm to 5 dBm. And, IF is 100 MHz. Kindly suggest me the IF power level for the given LO power levels.

    In my application, I want to use hmc554 in upconversion mode. Input LO is 13-18 GHz with the power of -2 dBm to 5 dBm. And, IF is 100 MHz. Kindly suggest me the IF power level for the given LO power levels. 

  • RE: HMC553ALC3B model on ADIsimRF

    Hi, you have a couple of options. You could pick a similar part such as HMC554 which has a minimum input frequency of 10 GHz. If you select this part and type in a frequency of 9400 MHz, the tool will accept this (it will give you a warning message) and…

  • HMC554ALC4B, HMC1081 simulation models

    Hello.

    I'd like to use both HMC554ALC4B and HMC1081 as mixer.

    I've got S-parametes about these chips...  but I have to know LO and IF and RF spurious... there are on HMC554's datasheet without HMC1081, moreover it's only for downconversion... I…

  • HMC554LC3B & HMC554ALC3B Comparison

    We've used the original Hittite Mixer for several years and now it's gone obsolete some time ago and need to provide customer justification and suitability for Analog Devices as a drop-in replacement.

    Can we please get a statement from ADI on…

  • RE: Passive double balanced mixer RF/LO port swap avalable?

    Hello,

    For the HMC554 the LO Drive level is +13dBm. The input P1dB is typically +11dBm so please keep the RF level below this for linear performance.

    For the HMC773 the LO Drive is also +13dBm. The input P1dB is typically +12dBm so please keep the RF…

  • 5月热点产品推荐,你最关注哪一款?

    5月,ADI主打5款产品——ADXL701、AD7124-8、HMC554、HMC649、HMC40x,有你关注或正在使用的产品吗?

    ADXL701——高精密、低g、数字Z轴加速度计,用于车辆侧翻检测和其它高性能应用。

    ADXL701在整个温度范围内提供高于±500 mg的偏置稳定性以及高于5%的灵敏度稳定性。 ADXL701设计采用可选的−3 dB滤波器转折频率,可满足各种应用,2 kHz的输出数据速率可对加速度信息进行充分过采样。


    特点和优势:

    • 高性能、z轴数字输出加速度计
  • Hittite RF - Machine & Charged Device Model Class

    Hi Tech support,

    Could you help to provide Machine and Charged Device Model Class on Hittite RF parts, see attached list.

    Thank you.

    Regards,

    HP