• RE: HMC553ALC3B model on ADIsimRF

    No particular reason. We have hundreds of parts and try to focus our efforts on modelling the newer parts. I can add HMC553 to the list of devices for the next release but that won't launch for a few months. 

  • RE: DC Offset Specs of Mixers

    Unfortunately the DC off set data you are requesting is not available.  I suggest you request an eval board for the HMC553 mixer.  This is the same mixer used in the HMC-C049.  This is a lower cost solution to determine what the DC offset is prior to buying…

  • Hittite RF - Machine & Charged Device Model Class

    Hi Tech support,

    Could you help to provide Machine and Charged Device Model Class on Hittite RF parts, see attached list.

    Thank you.

    Regards,

    HP

  • 12/16/2015: Full RF Signal Chains from 0Hz to 110GHz

    Presenter: Mel Conway, Product Manager, Instrumentation, High-speed & RF and Precision

     

    This webcast will explain ADI's new and expanded RF capabilities since the acquisition Hittite Microwave. We will give examples of the wider frequency spectrum…

  • 【在线研讨会讲义PPT下载】从0Hz到110GHz的全频谱RF信号链

    此次在线研讨会阐释了自收购Hittite Microwave后ADI的全新及扩展的RF能力。我们会举例说明ADI涵盖的更宽频谱范围及其真DC的重要性。信号链外的性能同样至关重要,展示低噪声、高稳定性控制和电源元件如何改善总体RF信号性能,并将讨论完整的信号链示例。

    主要讨论天线到比特和比特到天线,信号链覆盖,即刚才提到的从真正的DC 0 Hz到110 GHz的频谱覆盖。 我会简要介绍其中涉及到的各类设备。

    为什么良好的RF需要良好的电源,大家知道,RF需要干净的电源。然后,最后会和大家讨论“不止是芯片…