• HMC545A CONTROL QUESTION

    I want to use the HMC545A using a -7V/0V controls.  I can put inductors on the RF outputs to ground and also put blocking capacitors.   Will this work?
    Or no inductor but capacitors on the RF, will this work?    Basically I only have a negative supply and ground…

  • the amplitude of  HMC545A input signal

    Hello,

    In the application, the frequency of input signal is 0~500MHz, the amplitude is -5V ~ +5V. Can HMC545A be used in our application?

    Thank you,
    K

  • RF Switch Logic


    I want to confirm the logic of RF switch of models below:

    HMC595A

    HMC545A

    The truth table for them on RF1 & RF2 against A & B are reverse? can not direct replacement? Please advise.

  • RF switch logic

    Dear  Sir/Madam

    I want to confirm the logic of RF switch of models below:

    HMC595A

    HMC545A

    The truth table for them on RF1 & RF2 against A & B are reverse? can not direct replacement? Please advise.

    Thanks.

  • 又一次强强联手,ADI 的GaN技术有多牛?

    不久前,ADI公司宣布收购位于美国加利福尼亚州Santa Rosa的OneTree Microdevices公司,OneTree的GaAs和GaN放大器具有业内最佳的线性度、输出功率和效率,其丰富的专业知识积累,加之ADI公司在GaN技术上的战略重点,两大优势相结合,有利于扩展ADI公司面向基础设施、防务、仪器市场的高性能射频和微波信号链解决方案组合。

     

    (收购详情看这里:http://www.analog.com/cn/about-adi/news-room/press-releases/2017…