Hi,
Is there any chance that I can get the Touchstone file for HMC544A please?
Thanks
lham
Hi,
Is there any chance that I can get the Touchstone file for HMC544A please?
Thanks
lham
Hi,
I'm using an HMC544A evaluation board, with the control inputs driven from SN74AHC04 as shown in the data sheet.
When switching I see glitches like this (the glitch shown here is without RF applied for clarity, but I see the same thing if RF is…
Hello,
where can I download the gerber files of the evaluation board for HMC544A?
Can someone send me the files?
many thanks,
Dear all,
Currently, my customer has planned the product which uses HMC544A.
They need the Material Declaration of this chip.
Though I guided the following URL, two or more Material information is included there.
Hi,
I am working on a high speed data aquistion system. The low power RF signal of interest is DC coupled and therefore I was thinking of using the HMC544A as a switch. The datasheet looked promising (DC - 4GHz) until I have found the section that DC…
Hi all,
Our customer will try to use the RF SPDT SW @ low frequency circuit, about 1MHz ~ 50MHz.
They select following devices.
ADG902
HMC544A
HMC194AM
More performance data @ low frequency ~ 100MHz is available ?
P1dB,Isolation etc.
Best regards…
Hi there,
HMC544A's frequency range is specified from DC-4GHz. Unfortunately P1dB + IP3 parameters are only specified within 0.3-4GHz. My frequency region of interest is 2-100MHz. Does Analog Devices have the P1dB + IP3 specificaton in the mentioned…
Hi All,
One of my customer is considering ADF5130 RF Switch for his new design.
High frequency limit of 3.5GHz is okay for him, however, lower limit of 0.7GHz is too high for his application.
On the other hand, graph in Figure 5 through 9 shows the…
I was looking at LNAs and I cannot find anything in a reasonable price range. Probably something like BGA2866 will suit my needs.
Regarding 4 layers PCB here are the quotes:
Almost $60.
$27.
I think 2x price difference is huge. Even $27 for a hobby project…