• RE: HMC512 Vtune input impedance

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • VCO hmc778替代产品

    我们主要做分布式光电传感设备,之前用的VCO评估板型号为HMC778。想咨询使用这个产品来提供10.8G的电信号,参考输入0-350MHZ起到什么作用?

    HMC778被标注为新设计不推荐使用本产品,在同类型推荐中HMC512评估板,为什么没有参考输入和USB接口板来连接电脑?以及其HMC512的VTUNE接口如何连接电源?

    最后想问一下ADF5356评估板是否完美替代HMC778并适用我们的工作?

    谢谢大家,期待大家的回复。

  • transmission lines not covered with a solder mask

    Hi!

    Can you tell me, please, why didn't you cover the transmission lines in the CN0369 reference design (those, which are connected to the HMC512, for example) with a solder mask? What was the reason for not doing it?

    Thanks in advance!

    Best regards…

  • RE: Mistake in datasheet? (HMC787ALC3B)

    An additional example of the Line=RoHs is shown in the HMC512 datasheet, page 4, under package information. This is standard across all HMC products.  On plastic encapsulated parts, there may also be a suffix "E" for RoHs. Additionally, the ESD bag will…

  • Hittite VCOs from Analog Devices now available in ADIsimPLL

    The following Hittite VCOs from Analog Devices are now available in ADIsimPLL:

    v1.1:

    HMC507, HMC508, HMC509, HMC510, HMC511, HMC512, HMC513, HMC514, HMC515, HMC529, HMC530, HMC531, HMC534, HMC582, HMC583, HMC584, and HMC632.

    Added in v2.0:

    HMC391…

  • Where can I find software to synthesize a loop filter for legacy, HMC Integrated VCO / PLL Products?

    Many Analog.com users seem to be having difficulties finding evaluation board information and PLL design software to synthesize loop filter values loop bandwidth, settling time, integrated phase noise and more for the legacy HMC Integrated VCO/PLL products…

  • TAGS LIST: RF and Microwave

    HMC928
    HMC929
    HMC931
    HMC932
    HMC933
    HMC934
    HMC935
    HMC247G
    HMC538
    HMC-C018G
    HMC-C025G
    HMC-C053G
    HMC-C584G
    HMC7056G
    HMC7054G
    HMC7053G
    HMC7056AG
    HMC642G
    HMC642AG
    HMC643G
    HMC644AG
    HMC647
    HMC647A
  • 12/16/2015: Full RF Signal Chains from 0Hz to 110GHz

    Presenter: Mel Conway, Product Manager, Instrumentation, High-speed & RF and Precision

     

    This webcast will explain ADI's new and expanded RF capabilities since the acquisition Hittite Microwave. We will give examples of the wider frequency spectrum…

  • Equivalent Hours of HMC764LP6CE & HMC783LP6CE

    Dir Sir,

    I would like to know the equivalent hours of HMC764LP6CE & HMC783LP6CE. I cnn't find the information in the attached Reliability Report. How can I calculate that value?

    Best regards,

    Akira

  • 【在线研讨会讲义PPT下载】从0Hz到110GHz的全频谱RF信号链

    此次在线研讨会阐释了自收购Hittite Microwave后ADI的全新及扩展的RF能力。我们会举例说明ADI涵盖的更宽频谱范围及其真DC的重要性。信号链外的性能同样至关重要,展示低噪声、高稳定性控制和电源元件如何改善总体RF信号性能,并将讨论完整的信号链示例。

    主要讨论天线到比特和比特到天线,信号链覆盖,即刚才提到的从真正的DC 0 Hz到110 GHz的频谱覆盖。 我会简要介绍其中涉及到的各类设备。

    为什么良好的RF需要良好的电源,大家知道,RF需要干净的电源。然后,最后会和大家讨论“不止是芯片…