• ADF41513;HMC511;PLL合成器:ADIsimPLL仿真

    本人现在预使用ADI公司的两款芯片来实现某种频率合成器设计,分别为ADF41513和HMC511(VCO),滤波器使用有源无源振荡器,目前需要输出的频率范围为8〜13G左右,对于公司产品了解不深入以及仿真软件ADIsimPLL的使用不是很明了,同时对于仿真后的结果(噪声、杂散等)分析没有切入点,希望ADI专家能给一个类似的设计实例原理图或者解释让我参考一下吗

  • HMC511片子的17和24管脚有什么作用?

    技术专家,您好?在HMC511的datasheet中,17和24管脚是NO connection,我看到UG-383和UG-405中,给HMC511片子中17和24管脚带了很长的偏置电路?不知道有和作用?

  • 使用ADISimPll4.0对ADF4159及HMC511设计环路滤波器的问题

    拟采用ADF4159,HMC511,来产生9.55-9.56GHZ的锯齿波扫频信号,不知道ADISimPll4.0的设置不知道对不对?

  • RE: 签个到,送您好礼啦!(获奖名单已公布)

    西安 长安区  雷达FMCW  关注ADF4159 HMC511

  • RE: Equivalent Hours of HMC764LP6CE & HMC783LP6CE

    Hello Akira-san,

    The absence of test results for the HMC764LP6CE and HMC783LP6CE indicates that these devices were likely included in this report as products that were "qualified by similarity".  That means that they may not have actually been…

  • RE: Jitter data of HMC769LP6CE & HMC702LP6CE+HMC511LP5E(@9.4GHz)

    The Hitt-PLL tool can simulate phase noise at 9.1G and calculate jitter for the 10 KHz to 40 MHz integration limits.  The HMC769 model files are included as part of the tool installation package.  Set the output to 9.1G and change the Noise Integration…

  • Hittite VCOs from Analog Devices now available in ADIsimPLL

    The following Hittite VCOs from Analog Devices are now available in ADIsimPLL:

    v1.1:

    HMC507, HMC508, HMC509, HMC510, HMC511, HMC512, HMC513, HMC514, HMC515, HMC529, HMC530, HMC531, HMC534, HMC582, HMC583, HMC584, and HMC632.

    Added in v2.0:

    HMC391…

  • HMC703 (PLL) + HMC509 (VCO)

    I want to design a PLL using the HMC703 with an HMC509 or HMC511 VCO. I've been looking over the EVAL-HMC703LP4E schematic (which uses the HMC508 VCO) and associated datasheets. The output power of the HMC508 (and '509 and '511) is a little high (+10…

  • TAGS LIST: RF and Microwave

    HMC928
    HMC929
    HMC931
    HMC932
    HMC933
    HMC934
    HMC935
    HMC247G
    HMC538
    HMC-C018G
    HMC-C025G
    HMC-C053G
    HMC-C584G
    HMC7056G
    HMC7054G
    HMC7053G
    HMC7056AG
    HMC642G
    HMC642AG
    HMC643G
    HMC644AG
    HMC647
    HMC647A
  • Gerber Files for Catalog HMC VCO's in the LP5 package

    Question: Would it be possible to share the gerber files for the HMC1163 evaluation board?