• HMC498LC4 over 20mils Substrate

    I would like to use this amplifier inside new design made over 20 mils RO4350 substrate thickness. Without deembeded S-parameters it is quite hard to make it work well in wider bandwidth. 

    I would apreciate some help on this issue or some shared experience…

  • RE: HMC498-Die Performance at 200mA Drain Current

    Hello, What would be the Vgg to achieve the 250mA in Idd? I see there is information about this in otther model's datasheets but I could not find information for the HMC498LC4

  • RE: HMC499LC4 eval board gerbers

    Hi KSowronski942, 

    Gerber files for HMC499LC4 evaluation can be found on the product website (shown below) and through this link here: https://www.analog.com/media/en/technical-documentation/evaluation-documentation/gerber-files/HMC498LC4-HMC499LC4-HMC517LC4…

  • RE: DC block between HMC519 and HMC1019

    Hi Antoine,
    Regarding your scenario #1 from your email below:
    I support the HMC519LC4 and have in the past supported the HMC498LC4, so I can answer definitively for those two products. The HMC519LC4 and HMC498LC4 both have RFIN and RFOUT…
  • About the device S-parameters files

    About the device S-parameters files

    (HMC383LC4,HMC498LC4,HMC1040LP3CE,HMC1016)

    To whom it may concern:FormerMember

      We are going to design some PAs, using HMC383LC4,HMC498LC4,HMC1040LP3CE,HMC1016.

      These S-parameters…

  • EVB PCB design for Hittite devices.

    Hi all,

    Our customer need detailed layout guideline and PCB stack up guideline for the following devices.

    Are Gerber files available for the evaluation board?

    119667-HMC519LC4

    108537-HMC499LC4

    EVAL01-HMC1040LP3C

    EVAL01-HMC962LC4

    108537-HMC498L…

  • RE: HMC564LC4 Footprint

    Hi katsu,

    For the LC4 and LC4B footprints, please see attached.

    Also, the EVB Gerber files are now available on the product page (see direct link below):

    http://www.analog.com/media/en/technical-documentation/evaluation-documentation/gerber-files/HMC498LC4…

  • RE: RF Amplifer for Keysight Genesys

    The attached list details all of the ADI RF Amplifier Sys-Parameter models that are available in the 2015.08 release of Keysight Genesys.  This library will be updated over time.

       

    PartNumber RealPartNumber Description
  • 【在线研讨会回顾】雷达系统应用相关技术和解决方案

    新雷达系统采用各种不同的架构以满足多模式和多功能需求挑战。

    在我们近期举行的网络研讨会【雷达系统应用相关技术和解决方案】中,ADI应用工程师为大家介绍了采用L至Ku波段、RF采样系统、直接变频和超外差架构工作的雷达系统关键技术和解决方案。马上观看研讨会回放请点击:http://www.chinawebinar.com/landing/100224.HTM

    此次研讨会的完整讲义,下载附件查看。


  • RE: 36GHz RF oscillation signal source

    You need a PLL which drives a frequency doubler which drives an amplifier. Possible choices might be ADF4371 (PLL),  HMC1105 (frequency doubler) and HMC7229 (amplifier). These are not the only choices.

      PDF