• HMC465 chain biased with HMC980

    Hello,

    I have two HMC465 stages, biased at 8VDrain and 165mA  with the HMC980. The first stage seems to behave normally, however, the second stage causes a current alarm on the HMC980. The gate voltage is always at -1.8V even when the HMC980 is disabled…

  • ADS Non-linear models of Amplifiers (HMC1087, HMC465)

    Hi ,

    I am looking for the ADS Non-linear models of ADI Amplifiers in general and HMC1087 &  HMC465  in particular . Can you share these models if available.

    Thanks in advance 

    Satish 

  • HMC465 RF Amplifier VGG2 Voltage is out of spec.

    We are using the HMC465LP5 in our application; the bias to the device is provided by the HMC981 as per the recommended application circuit in the HMC981 datasheet.

     

    For our application, Vdd ~ +7.70V.  I have a sample of 4 units, and I have noted that…

  • 2HD, 3HD data of HMC441-Die and HMC462-Die

    Hi, 

    Could you share the 2nd and the 3rd harmonic distortion data?

    If there is no data of these products, something of the same product series is also fine.

    Regards,

    HM

  • ltc2641 die -

    The largest temp range the DAC will operate per the data sheet is -40 to +85 C. If I get the die will it operate at -55 to 125C? I will be mounting the die on ceramic substrate.

    does the assumption that it will work if properly heatsunk although the…

  • HMC939A-DIE

    Please provide S-parameters for HMC939A-DIE. Thanks.

  • Die Temperature

    How can I determine the die temperature of your device?

  • HMC341 die

    Where can I get the S parameter of LNA HMC341 measured on die? The S papameter offered on website is the results measured on test board.

  • HMC598 Die

    Hello,

    Do you have a maximum power consumption for the HMC598 in die form? The data sheet shows 175 mA @ 5 volts, but it's only a typical number and I'm seeing  220 mA @ 5volts, with no input signal or output load. Thanks.

    Best Regards.