• RE: 2HD, 3HD data of HMC441-Die and HMC462-Die

    Hi HM,

    Unfortunately, we do not have the 2nd & 3rd harmonic data for these parts (or the IP2 data required to calculate this) at the moment.

    Thanks,

    Dan

  • HMC462 Die RF Bond Pad Dimensions

    Hi, I would like to request for the RF bond pad dimensions of HMC462 die. 

    Please advise where I can find this info.

    Thank you very much and have a blessed day!

  • RE: HMC462

    Hi Kagan

    When you say this is a graph from "another HMC462 part", does this mean its

    just another version of the HMC462 product line and that doesn't match the

    die datasheet?  Or is this a completely different part and you are just

    showing…

  • HMC462 heatsink ???

    Good evening,

    Why should I mount the HMC462LP5 Testboard on a heatsink ?

    (As recommended in the datasheet, page 6, bottom)

    5V * 67 mA does not look like excessive heat.

  • how to get the hmc462's large signal model?

    how to get the hmc462's large signal model?

  • hello.how can i get the hmc462,s large signal model. thanks!

    hello.how can i get the hmc462,s large signal model. thanks!

  • RE: HMC-ALH435-DIE 10 Ohms on Vgg1

    Hi avatar,

    1) It's in series of the path.

    2)  I would recommend a bondable resistor from AVX.

    3) The resistor in between the bypass capacitors is part of the noise filtering bypass circuit and also is there to protect the gate .

    Thanks,

    DanO

  • ltc2641 die -

    The largest temp range the DAC will operate per the data sheet is -40 to +85 C. If I get the die will it operate at -55 to 125C? I will be mounting the die on ceramic substrate.

    does the assumption that it will work if properly heatsunk although the…

  • HMC939A-DIE

    Please provide S-parameters for HMC939A-DIE. Thanks.

  • Die Temperature

    How can I determine the die temperature of your device?