Hi,
What is the second harmonic rejection and OIP2 values of HMC460LC5 & HMC7950 amplifiers from 2-18GHz frequency range? Input power is -20dBm.
Hi,
What is the second harmonic rejection and OIP2 values of HMC460LC5 & HMC7950 amplifiers from 2-18GHz frequency range? Input power is -20dBm.
Hi opcirdes,
The Gerber files can be downloaded from the ADI website (download link below).
Thanks,
Dan
Hello,
I've two question regarding the evaluation board layout.
1) Can pins marked as N/C being connected to the ground(In evaluation board is so) ?
2) in evaluation board at the point that coplanar structure is connected to ic pin the central connector…
Q: What is the purpose of the 2.2 uF || 1000 pF decoupling capacitance on the VGG pin of HMC460LC5?
I need to know what is the absolute maximum rating for Idd. I fond in the data sheet typical Idd=75mA but nothing about its absolute maximum rating ...
Best regards
Hi
I found the attached file on EngineerZone.
Q1: Is this the latest and greatest biasing circuit for the HMC460LC5?
Q2: How is VGate calculated and what is its value?
Thanks,
Kind regards,
Paul.
.PDF
Hi,
The amplifier OIP2 data is not available in datasheet, Please provide the same to estimate the IMD2 and 2nd harmonics levels.