• HMC406 Issue

    HI,

    I was testing HMC406 amplifier.

    I am facing issue of HMC406. It is drawing too much current almost 600mA. Even we tried to control the VDD current by adjusting VPD. But even then problem persists. With Vpd = 0 also current drawing 500mA. Please…

  • HMC406 for single ended output application

    Hi,

    Any idea on how to design HMC406 as single output instead of dual output?

    1. Do I need to insert a 50 ohm termination for unused pin?

    2. Short pin 5 and pin 6 to get single output?

  • the input and output matching problem HMC406

    I am facing problem in matching the input port of HMC406 to 50 ohm at 5.6 GHz.

  • Can the HMC406 be matched to work from 4.4-5.1 GHz?

    The HMC406 is intended to be used from 5-6 Ghz. The S11 seems to be optimized for 4.4-5.1 GHz based on the S-parameters provided. Can the S22 be matched to 4.4-5.1 GHz?

  • Looking for S-Parameters

    Where can I find s-parameters for the following devices?

    AD8340

    HMC1040

    ADAR2001

    ADPA1122

    HMC406

  • RE: FAQ: ADI PA replacement of Skyworks PA SE5004L

    A: The closest match in terms of performance is HMC408 but it has higher quiescent current draw than the Skyworks part. There are lower output power alternatives that also have lower quiescent current (HMC406, HMC407 and HMC415)

  • RE: HMC406MS8G

    Hi Sundaravalli,

                              S-Parameters are available for download on the HMC406 product page. I've attached the link for you.

    https://www.analog.com/media/en/simulation-models/s-parameters/HMC406MS8G.zip

    Regards,

    Jim B

  • 5月热点产品推荐,你最关注哪一款?

    5月,ADI主打5款产品——ADXL701、AD7124-8、HMC554、HMC649、HMC40x,有你关注或正在使用的产品吗?

    ADXL701——高精密、低g、数字Z轴加速度计,用于车辆侧翻检测和其它高性能应用。

    ADXL701在整个温度范围内提供高于±500 mg的偏置稳定性以及高于5%的灵敏度稳定性。 ADXL701设计采用可选的−3 dB滤波器转折频率,可满足各种应用,2 kHz的输出数据速率可对加速度信息进行充分过采样。


    特点和优势:

    • 高性能、z轴数字输出加速度计
  • TAGS LIST: RF and Microwave

    HMC928
    HMC929
    HMC931
    HMC932
    HMC933
    HMC934
    HMC935
    HMC247G
    HMC538
    HMC-C018G
    HMC-C025G
    HMC-C053G
    HMC-C584G
    HMC7056G
    HMC7054G
    HMC7053G
    HMC7056AG
    HMC642G
    HMC642AG
    HMC643G
    HMC644AG
    HMC647
    HMC647A
  • Need BOMs of each HMC EVB

    Dear,

    Can you please help to get BOM(Bill of Materials) file of below each EVB ?

     

    EVAL-HMC406MS8G

    EVAL-HMC408LP3

    EVAL-HMC425LP3

    EVAL-HMC624ALP4

     

    I found HMC425A. This part is pre-released part. Can I get release schedule ?

     

    Thanks a lot.