• ADRF5424 Die Form

    Hi,

    Is ADRF5424 available in die form?

    What does Die on Carrier means?

    Thank you.

  • HMC797A-Die

    Hi,

    Is it possible to maintain RF ON while the amplifer is OFF?

    Thank you so much

    Chiara

  • ADRF5044 DIE

    Is this product available in DIE form?

    Thanks

  • ADPA 7008 and ADPA 7009 die attachment

    We would like verify the die attachment method for ADPA 7008 & 7009 is epoxy.

    Is there anything in particular we need to use? Any brand suggestions or recommendations?

  • HMC-ABH241 : Die Related- Queries

    Find both Q&A below. 

     

    1. We only show decoupling for one side of the die. The top side in the view
    below has the same supply pads. Is decoupling only on one side required and can
    it be either side?
    Yes the supplies only on south or north side can…

  • DIE level parts?

  • ADL6010 bare die temperature range

    The packaged variants of the ADL6010 comparator include devices that are rated for a -55C to +125C temperature range.  There is also a space qualified version of this device (ADL6010s-DIE) that is rated for -55C to +125C.  I need a die part with a -55C…

  • HMC8402-DIE S-Parameter

    Hi,

    What is the impact of the measurement method on HMC8402-DIE S-Parameter values?

    I found a similar question and replies about HMC-AUH312. (please refer to the following URL)

     https://ez.analog.com/rf/f/q-a/542638/hmc-auh312-s-parameter 

     Is it OK to assume…

  • AD777x: How can the temperature of the die be calculated?

    In the datasheet the equation to calculate the temperature can be found.
    This equation calculates the temperature rise referred to 25°C, so to calculate the absolute temperature it is necessary to add 25° to the previous equation:
    The DVbe…
  • ADAU1451WBCPZ - Unconnected IO from die to IC pin

    Hi,
    Could you please confirm that whether the DSP(ADAU1451WBCPZ) has  unconnected I/O which is physically on the die but not bonded to pins.
    Please provide the information as soon as possible.

    Thanks in advance