• AD9162-FMCB-EBZ latest Schematics

    My customer bought the EVAL-AD916X evaluation board.(AD9162-FMCB-EBZ)


    My customer says as follows.
    The actual circuit board is different from the schematic  downloaded from the wiki page.
    U 37 HMC 365S8GE is actually HMC362.
    Y61 122.88 M is actually 120…

  • RE: HMC948 Enable Pin and Package

    hi Eike,

    Pin 12 is a not connected internally.

    There's no die version of HMC948. HMC611 is available in die, but up to 10ghz.

    -andy

  • HMC341 die

    Where can I get the S parameter of LNA HMC341 measured on die? The S papameter offered on website is the results measured on test board.

  • ltc2641 die -

    The largest temp range the DAC will operate per the data sheet is -40 to +85 C. If I get the die will it operate at -55 to 125C? I will be mounting the die on ceramic substrate.

    does the assumption that it will work if properly heatsunk although the…

  • HMC939A-DIE

    Please provide S-parameters for HMC939A-DIE. Thanks.

  • HMC392A-Die

    I wanted to Simulate the HMC392A in Microwave office. So i downloaded its S2P file from design resources and as i performed simulation its responses like return loss is better than the datasheet but its gain is decreased to max15.7 dB after simulation…

  • Die Temperature

    How can I determine the die temperature of your device?

  • HMC598 Die

    Hello,

    Do you have a maximum power consumption for the HMC598 in die form? The data sheet shows 175 mA @ 5 volts, but it's only a typical number and I'm seeing  220 mA @ 5volts, with no input signal or output load. Thanks.

    Best Regards.

  • HMC588LC4BTR two die code

    I bought HMC588LC4BTR   from Arrow on line  1805+  and another Chinese agent 1812+,

    because there is somthing differences on the labels 

    Therefore, I have tested the goods through the white horse inspection agency in China and the AAA inspection agency in the…

  • HMC347A-Die v.s. HMC347B

    Hi all,

    Our customers have used HMC347.
    They will consider choosing a replacement product as the stock purchased at the last time buy will be gone.
    HMC347A-Die and HMC347B are both dies, and there is a difference between suffixes A and B.
    I do not know why…