Hello,
Can you please tell me if the HMC347 is subject to hydrogen poisoning?
Thanks.
I have a few questions regarding the HMC347 Control Voltage.
1.) Do you have min. max. threshold voltages for the control logic?
2.) What happens to the switch performance when control voltages are between 0 and -5, say -4V, -3V, -2V, or -1V…
I'm looking to control four HMC347 die devices using the same driver, could you please tell me the resistance and capacitance for the A / B control inputs? Also would you have switch time numbers above 90%RF? Thanks.
Best Regards.
Hi all,
Our customers have used HMC347.They will consider choosing a replacement product as the stock purchased at the last time buy will be gone.HMC347A-Die and HMC347B are both dies, and there is a difference between suffixes A and B.I do not know why…
HI,could you help to show low frequency(100k-300MHz) P1dBout performance of hmc347,hmc460LC5,HMC797A?
We can't find relative data description in datasheet.Thanks!
图一
图一中U2是ADF4351,U6和U8是两个串联的射频开关HMC347,两个开关中心距是6mm,一个HMC347在2.4GHz隔离度大概50多dB,C44这边是ADF4351频率源的输出,是个连续的2.42GHz信号,功率是0dBm,2个HMC347开关在同一个FPGA控制信号的控制下形成一个20ns宽的矩形脉冲,矩形脉冲内截取的是一段20ns宽的ADF4351的2.42GHz正弦波,但是在2个HMC347都关断的情况下,C74这边居然还有-40dBm的2.42GHz信号,如图二,
图二…
I receuved an inquiry about SW control of HMC347 from our customer.
The Control Input is defined two types (A:High/B:Low and A:Low/B:High) on the datasheet.
Are there any problem if A & B is Low or A & B is High transiently?
Best Regards…