• HMC341 die

    Where can I get the S parameter of LNA HMC341 measured on die? The S papameter offered on website is the results measured on test board.

  • RE: ADuCM355 Using AFE Clock for Digital Die

    Hi Yan-Wei,

    A couple of points to note:

    - The digital die maximum clock rate is 26MHz. This is the max clock rate the memories and digital logic were tested and qualified to. 

    - Did you follow the steps in the user guide under the section "Connecting AFE…

  • ltc2641 die -

    The largest temp range the DAC will operate per the data sheet is -40 to +85 C. If I get the die will it operate at -55 to 125C? I will be mounting the die on ceramic substrate.

    does the assumption that it will work if properly heatsunk although the…

  • Die Temperature

    How can I determine the die temperature of your device?

  • HMC392A-Die

    I wanted to Simulate the HMC392A in Microwave office. So i downloaded its S2P file from design resources and as i performed simulation its responses like return loss is better than the datasheet but its gain is decreased to max15.7 dB after simulation…

  • HMC939A-DIE

    Please provide S-parameters for HMC939A-DIE. Thanks.

  • HMC598 Die

    Hello,

    Do you have a maximum power consumption for the HMC598 in die form? The data sheet shows 175 mA @ 5 volts, but it's only a typical number and I'm seeing  220 mA @ 5volts, with no input signal or output load. Thanks.

    Best Regards.

  • HMC6981LS6 Die dimensions

    Hello,

    I am conducting thermal analyses in Ansys Icepak on a board with some HMC6981LS6 amplifiers on it.

    To properly model the amplifiers, I need to know the dimensions of the die, the die attach and the die pad, which I couldn't find on the datasheet…

  • RE: LTC2000 Operating Temperature vs Junction temperature

    The 70C is referring to the temperature of the die. Keep the die lower than 70C with a heatsink or use a higher temperature grade. 

  • RE: RH1814 Thermal Resistance

    I need to predict the junction temperature of the die (bare die soldered onto a board). Do you have any test data or thermal resistance data that would be relevant? If you have a theta JC for a packaged version of this die, I would also be interested…