• HMC6981LS6 Die dimensions

    Hello,

    I am conducting thermal analyses in Ansys Icepak on a board with some HMC6981LS6 amplifiers on it.

    To properly model the amplifiers, I need to know the dimensions of the die, the die attach and the die pad, which I couldn't find on the datasheet…

  • RE: LT3080 Exposed Pad Is Soldered to Ground by Mistake

    The bottom of the LT3080 die is supposed to be a resistive version of the OUT pin.  I say “supposed to be” because in reality there is a thin layer of unavoidable but inadvertent oxide between the die silicon and the exposed pad metal.  That…

  • HMC341 die

    Where can I get the S parameter of LNA HMC341 measured on die? The S papameter offered on website is the results measured on test board.

  • Die Temperature

    How can I determine the die temperature of your device?

  • ltc2641 die -

    The largest temp range the DAC will operate per the data sheet is -40 to +85 C. If I get the die will it operate at -55 to 125C? I will be mounting the die on ceramic substrate.

    does the assumption that it will work if properly heatsunk although the…

  • HMC392A-Die

    I wanted to Simulate the HMC392A in Microwave office. So i downloaded its S2P file from design resources and as i performed simulation its responses like return loss is better than the datasheet but its gain is decreased to max15.7 dB after simulation…

  • HMC939A-DIE

    Please provide S-parameters for HMC939A-DIE. Thanks.

  • HMC598 Die

    Hello,

    Do you have a maximum power consumption for the HMC598 in die form? The data sheet shows 175 mA @ 5 volts, but it's only a typical number and I'm seeing  220 mA @ 5volts, with no input signal or output load. Thanks.

    Best Regards.

  • RE: Questions of different label, x-ray inspection and die structure

    Hello J.C.,

    Here is a response from folks within ADI who looked at your questions:

    "They are comparing the old die revision to the new die revision material.  The PCN effectivity date is only a marker to the earliest possible date of conversion and…

  • RE: HMC129 part compatibility 1997rev and a 2007 rev part

    Hi,

    Firstly if the HMC129 is going to be used for a new design then please be aware that this part is not recommended for new designs.

    The 2 die are different due to a process change. The performance between the 2 die should be similar (isolation).…