• HMC321A release date

    when will the HMC321A release to production?

    _Tim Starr on behalf of BW@LG

  • hmc321a use problem

    I am using evaluation board of hmc321a. From the data sheet, it meets the requirement of bias current between 4mA and 8mA when I supply 5V voltage at V port.Why does it burn out? And as the above picture shows, Does the red circle indicate the location…

  • HMC321A control signal Vih_min value

    The preliminary HMC321A SP8T RF switch datasheet states that the control interface uses a "positive control voltage of
    0/+5 volts" but no further information is given.  Looking at the datasheet for the existing HMC321 part the control voltages…

  • HMC321A RF Signal Amplitude

    I need to switch a number of RF signals that are 200Mhz at up to +3V peak to peak. There is no specification on the max AC voltage level of the RF inputs. Will the HMC321A work in this application?

  • HMC321A switch - maximum pulsed input power

    Hi,

    we are using HMC321A for an application using WiFi signals at 5GHz, based on OFDM modulation. Using a signal generator from R&S, I have tried to increase the average input power up to +9dBm (which corresponds to ~20dBm PEP - Peak Envelope Power)…

  • RE: EV1HMC321ALP4E-SP8T switch Broken after one time measurement

    Hi,

    HMC321A was fully tested and specified with nominal Vdd supply of 5V. It can still be operated down to 3V supply but there will be degradation in large signal performances. However HMC321A may not be functional and reliable when it is powered with…

  • RE: Is the HMC321ALP4E bidirectional?

    Hi,

    HMC321A is bidirectional. It can be used to transmit signal in both way, from RFC to RFx or RFx to RFC.

    Best.

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225
  • HMC321 response time delay

    Hello I'm RF engineer.

    I'm using HMC321 to divide RF band.

    When I change the path RF1 to RF2, It need some delay time.

    It doesn't mean switching time, the time is reaching final value of settling time 0.05dB(98.86% of the final value).

    Now…