• The RF signal amplitude output of HMC264LC3B.

    The RF signal amplitude output of f HMC264LC3B is too low, which is 20dB lower than that of subharmonic.

    you can see RF signal at 26.05GHz(-47.56dBm) when LO=13GHz (-4dBm), IF = 0.05GHz (-8.44dBm) .

    But the amplitude of subharmonic(26GHz) is -20dBm.

  • The peripheral reference circuit of hmc264lc3b.

    The peripheral reference circuit of this chip is not in the data sheet, can you provide it?  

    Think you.

  • 108779-HMC264LC3B ,PCB Mount SMA Connector

    Hi all,

    RF Frequency Range @ hmc264lc3b is 22 - 31 GHz.
    J1 - J3 PCB Mount SMA Connector is true ?
    PCB Mount SMA Connector of J1 RF input is same as J3 IF and J2 LO ?
    Isn't 2.92mm PCB Mount K-Connector appropriate for J1 RF?

    Best regards,

    sss

  • HMC264LC3B ADS simulation

    We are a group of 5 students who a making a LOE satellite ku/ka-band receiver/transmitter system. It is for a semester project at Aalborg university where we are studying a master in wireless communication systems. For efficient development the system…

  • HMC264LC3B Spurious issue

    Hello,

    I received a support request about HMC264LC3B from our customer. The customer has used HMC264LC3B as an up-converter for their system and he has a spurious issue.  

    For example,

     he can see spurious at 28.02GHz when LO=12GHz (-4dBm), IF  = 3.99GHz …

  • EVB PCB design for Hittite devices.

    Hi all,

    Our customer need detailed layout guideline and PCB stack up guideline for the following devices.

    Are Gerber files available for the evaluation board?

    119667-HMC519LC4

    108537-HMC499LC4

    EVAL01-HMC1040LP3C

    EVAL01-HMC962LC4

    108537-HMC498L…

  • RE: 36GHz RF oscillation signal source

    You need a PLL which drives a frequency doubler which drives an amplifier. Possible choices might be ADF4371 (PLL),  HMC1105 (frequency doubler) and HMC7229 (amplifier). These are not the only choices.

      PDF

  • RE: Query

    This part is EAR99. The attached RFIC selection guide lists the ECCN codes for all of ADI's RF products.

     PDF