• HMC341 die

    Where can I get the S parameter of LNA HMC341 measured on die? The S papameter offered on website is the results measured on test board.

  • HMC598 Die

    Hello,

    Do you have a maximum power consumption for the HMC598 in die form? The data sheet shows 175 mA @ 5 volts, but it's only a typical number and I'm seeing  220 mA @ 5volts, with no input signal or output load. Thanks.

    Best Regards.

  • What is Monotonic performance of the HMC247 ?  Precisely what is the phase linearity with control voltage at any given RF input Frequency?   Nagamayya

    What is Monotonic performance of the HMC247 ? Precisely what is the phase linearity with control voltage at any given RF input Frequency? Nagamayya

  • RE: HMC985A-Die rf pins interchangeability

    Hi,

    HMC985A-Die can support bi-directional operation, however, the power handling for RFOUT might be lower than RFIN.

    The absolute max RF input power for HMC985A-Die is 30dBm as listed in the datasheet, therefore, I think it is OK to apply 15dBm max to…

  • HMC392A-Die

    I wanted to Simulate the HMC392A in Microwave office. So i downloaded its S2P file from design resources and as i performed simulation its responses like return loss is better than the datasheet but its gain is decreased to max15.7 dB after simulation…

  • HMC6981LS6 Die dimensions

    Hello,

    I am conducting thermal analyses in Ansys Icepak on a board with some HMC6981LS6 amplifiers on it.

    To properly model the amplifiers, I need to know the dimensions of the die, the die attach and the die pad, which I couldn't find on the datasheet…

  • AD8515: Die size

    Are these dies AD8515 and OP284CHIPS smaller than 1 x 1 mm²? That would be an
    absolute max for us.

     

    1. The OP284CHIPS has a die size of 1.620 mm x 2.301 mm.
    2. The AD8515 has a die size of 0.660 mm x 0.920 mm.

    Therefore only the…
  • ADG5206 bare die

    Hi,

    Currently we are using ADG5206 (LFCSP_WQ package) and we are looking for ways to decrease the required footprint per channel. One way would be using bare dies. As there is a list of "as bare die" available products ( http://www.analog.com…

  • Pluto SDR in Ethernet Adaptor Mode Randomly Has Adaptor Die

    Hi all,

    I am noticing that occasionally, the ethernet adaptor I am using with my Pluto randomly has no lights.  At that point, I have no way to get into the Pluto to troubleshoot.  This happens after the Pluto has been sitting idle with no TX or RX activity…

  • AD8354 bare die

    Hello,

    Do you sell this amplifier as a bare die,  without the package?

     Thank you in advance,