Q: Can you share any information on the bond pad metallization and passivation for HMC1126?
Q: Can you share any information on the bond pad metallization and passivation for HMC1126?
Please provide the following information for both the parts HMC1126 and HMC1127:
Hi
Regarding HMC1126 D/S, the power up/down sequence is recommended as follows.
Power up : GND -> VGG1 -> VDD -> VGG2 -> IDQ -> RF signal
Power down : RF signal -> IDQ -> VGG2 -> VDD -> VGG1
Is it possible for VDD and VGG2 to…
Dear team,
Our customer is using the I am reviewing the LNA for the Test & Measurement.
I am suggesting the HMC8401 and HMC1126 for the Test and Measurement application.
I have received some technical inquiries.
1. test data for Gate current(Igg1) Vs…
Hello,
I need S2P data for the HMC1126 and HMC1127. If Hittite has Gain/oP1dB/oIP3/oIP2 vs frequency and Vdd in
excel format that would also be helpful too.
I also need a data sheet on the HMC7149 amplifier along with some (maybe excel format) data…
I’d like to calculate the frequency dependent noise figure and OIP3 of a composite system I am simulating. Would it be possible to get the raw data behind the follow plots from the following datasheets?
Dear team,
I am using the HMC1126 for Test and Measurement.
I would like to know the resistance value of RF input and output port.
According to the interface schematics of datasheet, there are DC blockign capacitors inside. So I think that RF input and…
Hi Chris,
I will upload a file so you can get the correct structure of the mdf file.
Re
!HMC1049LP5E !HMC1126 BEGIN data !TEST CONDITIONS: Vd = 5.0V; Id = 65mA;…
当今世界上存在许多涵盖不同频率范围的电信标准。利用宽带放大器实现的RF系统解决方案可以通过一个产品涵盖多个频段,从而降低系统成本并减小尺寸。
近期举行了一场主题为《使用宽带放大器满足电信多频段需求》的在线研讨会。在研讨会中,我们介绍宽了带放大器的关键性能参数和所需偏置策略,从而实现最佳的放大器RF性能。观看研讨会视频请点击:http://seminar.eepw.com.cn/seminar/show/id/283
这里也分享下此次研讨会的讲义,共大家下载参考学习哦
消息编辑者为…
The attached list details all of the ADI RF Amplifier Sys-Parameter models that are available in the 2015.08 release of Keysight Genesys. This library will be updated over time.
PartNumber | RealPartNumber | Description |